STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4066 Views
  • 0 replies
  • 3 kudos

I want to control a remote controlled car, could you advise me what is best to use? I had thought about the 5G that is present in my city but I don't know if it is a good idea. I would also need to receive the audio and video signal

 I had thought about the 5G that is present in my city but I don't know if it is a good idea. I would also need to receive the audio and video signal. is it possible to make?

Alfred04 by Associate
  • 681 Views
  • 0 replies
  • 0 kudos

Unknown aci_gatt_proc_complete_event

I am getting this event upon sending : ACI_GATT_EXCHANGE_CONFIGI can't understand why I am getting it. What procedure is complete?According to AN5270 I should not get it for that command.

0693W00000VOBljQAH.png
DS.4 by Senior II
  • 1058 Views
  • 1 replies
  • 0 kudos

GPIOB not enabled on STM32WL55JC2

Hello, I just received my WL55JC2 card and I would like to blink one of the leds on the card with a very simple line of code but I don't understand why it doesn't work. I noticed that the led was pinned on the GPIOB which was not enabled in the gener...

0693W00000VO8rjQAD.jpg 0693W00000VO8roQAD.jpg 0693W00000VO8rtQAD.jpg 0693W00000VO8s8QAD.jpg
BNamu.1 by Associate II
  • 1051 Views
  • 1 replies
  • 0 kudos

Resolved! Over the air (OTA) firmware update for STM32WLE5xx MCUs

Hello,The datasheet for STM32WLE5xx states, that this series is capable of OTA firmware update, however I am not able to find any resources on how do perform it. The only document that shows up is the AN5554 application note on firmware update over t...

MLisa.1 by Associate
  • 1985 Views
  • 2 replies
  • 0 kudos

STM32WB5MMG short-range joining network

Zigbee test using 1xZC and 1xZR.For ZR to join network, the distance to ZC was limit to arround 2m. After join network, the distance ZR message to ZC can be extended to about 20m.​Not understand why the join distance so short. ​Here's my test setup: ...

ZChen.6 by Associate
  • 1162 Views
  • 1 replies
  • 0 kudos

How to save LoRa key context into the flash so that it don't have to send the join request every time it wakes up or restart?

Hi! I'm working on STM32WLE5JC micro-controller. Is there any way to write the firmware in such a way that I don't have to send the join request every time the controller wakes up or restarts?I mean when I first time join the network, what are the sp...

0693W00000Uo58AQAR.png
MAwan.1 by Associate
  • 2004 Views
  • 2 replies
  • 0 kudos