I attended the Tuesday Sept 7th session of the lorawan-with-stm32wl-soc-workshop-ame-2021 I was unable to complete the workshop during the allotted time. I would like to complete the training. Are the videos available?
Posted on June 11, 2017 at 20:47♯ build using ♯&sharpen.X-CUBE-SPN7.zip Running an up-to-date Eclipse Ac6 session here is what happens when I try to build the &sharpX-CUBE-SPN7 demo application:1.select File menu item2. select Open Projects from...
Thanks. That works for joining today's session, which terminates in about a half hour. I'm not set up. I still will need to work through the seminar after setting everything back up.Can i download or access the 87 min video off-line?
Posted on September 28, 2017 at 02:25The 1.1.0 release of SPN7 on the website resolves two issues:1. Importing the project sets up correct file paths so the project can be built.2. SW4ST/Ac6 builds a F302R8 binary file that fits in the F302R8 memor...
Posted on June 21, 2017 at 04:38Thanks for the tip on changing the project file to denote the filelocations. That suggestion worked. The 302R8 code compiles with the patchto the project file applied.However it is too big for a 302R8. The compiled co...