STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Hi, I am using the STM32WB55 custom board as a client. My Task is to create a connection with the server when a button is pressed. and send the write attribute command and then disconnect from the server immediately.

Steps I am following:Scan for the server and get the MAC of the serverWhen the button is pressed call aci_gap_create_connection to start the connectionThen write the attribute and disconnect from the server.Hear the problem I am facing is it takes 3s...

AM.12 by Associate III
  • 1889 Views
  • 5 replies
  • 0 kudos

Using STM32WB for bidirectional smartphone application

I developed a prototype using a UART to Bluetooth dongle, the HC-05. This worked like a charm. I could pair my smartphone to it and continuously send data between the MCU Board and my smartphone. Now I want to optimize size and cost, therefore I choo...

YGail.2 by Associate III
  • 1746 Views
  • 2 replies
  • 2 kudos

STM32WB for low latency wireless mouse application

As the title says, I want to create a wireless mouse and was wondering if it was possible to make a low latency mouse using two STM32WBs (one for the mouse and one for the computer). Is this possible with this MCU series or is it better to use a dedi...

I want to configure B-L072Z-LRWAN1 Board-1 to transmit data through USB device(CDC) and another board-2 to receive data through LoRa, if board-2 after receiving data, if it send some data then board-1(which is connected to PC) have to receive it.

Between Board 1 and Board 2 data exchange should be done through LoRa and data exchange between Board 1 and PC should be through USB. It would be very helpful if someone help with this.

Error: failed to erase memory

I'm using LoRa E5 mini board that has STM32WLE5 MCU on it.I use STM32CubeProgrammer and the STlink of a Nucleo64 board to send the firmware to it.For some boards, I cannot succeed to flash them and get this error : When I try to use STM32CubeIDE I've...

0693W00000Y8XmyQAF.png 0693W00000Y8XncQAF.png
Hugo_VOLA by Associate II
  • 5184 Views
  • 3 replies
  • 0 kudos