cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB5MM ble freertos project - Issue with CPU2 initializzation

GPomp.1
Associate III

Hi support, 

I'm working with STM32WB5MM, the application is a ble application with freertos. 

I have this issue, sometimes at the boot the MX_APPE_Init() fails. In the details, the fuction APP_BLE_Init( void ) isn't executed because the function APPE_SysUserEvtRx() is never called. 

I try without success to:

1) Increase the minimun stack size (setting to 0x1000) and minimum heap size (setting to 0x400)

2) Increase the priority of the following interrupt: IPCC RX, IPCC TX

I attach the code of the main function:

int main(void)

{

 /* USER CODE BEGIN 1 */

  /**

  * The OPTVERR flag is wrongly set at power on

  * It shall be cleared before using any HAL_FLASH_***() api

  */

 __HAL_FLASH_CLEAR_FLAG(FLASH_FLAG_OPTVERR);

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */

 HAL_Init();

 /* Config code for STM32_WPAN (HSE Tuning must be done before system clock configuration) */

 MX_APPE_Config();

 /* USER CODE BEGIN Init */

 //Reset_Device(); // BLE_ADD

 //Config_HSE(); // BLE_ADD

 /* USER CODE END Init */

 /* Configure the system clock */

 SystemClock_Config();

 /* IPCC initialisation */

  MX_IPCC_Init();

 /* USER CODE BEGIN SysInit */

 //MX_IPCC_Init(); // BLE_ADD

 PeriphClock_Config(); // BLE_ADD

 //Init_Exti(); // BLE_ADD /**< Configure the system Power Mode */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */

 MX_GPIO_Init();

 MX_ADC1_Init();

 MX_COMP1_Init();

 MX_I2C1_Init();

 MX_LPUART1_UART_Init();

 MX_USART1_UART_Init();

 MX_SAI1_Init();

 MX_SPI1_Init();

 MX_SPI2_Init();

 MX_TIM1_Init();

 if (MX_FATFS_Init() != APP_OK) {

  Error_Handler();

 }

 MX_USB_Device_Init();

 MX_IWDG_Init();

 MX_RTC_Init();

 MX_RF_Init();

 /* USER CODE BEGIN 2 */

 Configure_PWR();

 HAL_NVIC_DisableIRQ(EXTI9_5_IRQn);

 HAL_NVIC_DisableIRQ(EXTI4_IRQn);

 HAL_NVIC_DisableIRQ(EXTI15_10_IRQn);

 HAL_NVIC_DisableIRQ(SPI1_IRQn);

 HAL_NVIC_DisableIRQ(COMP_IRQn);

 HAL_UART_AbortReceive(&huart1);

 HAL_UART_AbortTransmit(&huart1);

 HAL_UART_AbortReceive_IT(&huart1);

 HAL_UART_AbortTransmit_IT(&huart1);

 HAL_UART_AbortReceive(&hlpuart1);

 HAL_UART_AbortTransmit(&hlpuart1);

 HAL_UART_AbortReceive_IT(&hlpuart1);

 HAL_UART_AbortTransmit_IT(&hlpuart1);

 /* USER CODE END 2 */

 /* Init scheduler */

 osKernelInitialize();

 /* USER CODE BEGIN RTOS_MUTEX */

 /* add mutexes, ... */

 /* USER CODE END RTOS_MUTEX */

 /* Create the semaphores(s) */

 /* creation of imuAccessSemaphore */

 imuAccessSemaphoreHandle = osSemaphoreNew(1, 1, &imuAccessSemaphore_attributes);

 /* creation of txDebugSemaphore */

 txDebugSemaphoreHandle = osSemaphoreNew(1, 1, &txDebugSemaphore_attributes);

 /* USER CODE BEGIN RTOS_SEMAPHORES */

 /* add semaphores, ... */

 /* USER CODE END RTOS_SEMAPHORES */

 /* USER CODE BEGIN RTOS_TIMERS */

 /* start timers, add new ones, ... */

 /* USER CODE END RTOS_TIMERS */

 /* USER CODE BEGIN RTOS_QUEUES */

 /* add queues, ... */

 /* USER CODE END RTOS_QUEUES */

 /* Create the thread(s) */

 /* creation of defaultTask */

 defaultTaskHandle = osThreadNew(StartDefaultTask, NULL, &defaultTask_attributes);

  

 /* USER CODE BEGIN RTOS_THREADS */

 /* add threads, ... */

 /* USER CODE END RTOS_THREADS */

 /* Create the event(s) */

 /* creation of generalEvent */

 generalEventHandle = osEventFlagsNew(&generalEvent_attributes);

 /* creation of xCreatedEventGroupSystem */

 xCreatedEventGroupSystemHandle = osEventFlagsNew(&xCreatedEventGroupSystem_attributes);

 /* USER CODE BEGIN RTOS_EVENTS */

 /* add events, ... */

 xEventGroupClearBits(xCreatedEventGroupSystemHandle, init_Board_done_BIT );

 xEventGroupClearBits(xCreatedEventGroupSystemHandle, ble_init_BIT );

 /* USER CODE END RTOS_EVENTS */

 /* Init code for STM32_WPAN */

 MX_APPE_Init();

 /* Start scheduler */

 osKernelStart();

 /* We should never get here as control is now taken by the scheduler */

 /* Infinite loop */

 /* USER CODE BEGIN WHILE */

 while (1)

 {

  /* USER CODE END WHILE */

  /* USER CODE BEGIN 3 */

 }

 /* USER CODE END 3 */

}

What should be the issue? Can you give me any suggestion for try to solve this problem?

Regards,

Giampietro

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Hello Giampietro,

Have you found a solution to this issue? I'm noticing a similar issue that APPE_SysUserEvtRx() isn't called. I do notice that it sometimes works depending on my compiler optimization settings, but its seems very non-deterministic.

FreeRTOS appears to initialize just fine, but the APPE_SysUserEvtRx callback does not trigger.

Best,

Patrick