NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
How can I check the ATT-MTU of the current connection (not setup)?What coding can I use to check? For example, I want to return ATT-MTU size through USART after measuring it in the microcontroller.
During several trial to use ACI_GATT_Write_Long_Char_Value,I found that the microcontroller dosen't start its BLE advertisement anymore.It only can indicate wireless firmware version.I think that some transmission cause an error.So, I tried to rewri...
HI everyone, I'm working on creating a sequence of files, that everytime the program starts to run, it creates a sequential file of the last one created. But I'm having troubles trying to create a logic that compares the name of the last file and cre...
Hi.I can see that CFGBSY bit is set and reset in some MX peripheral init functions, but the main problem is that it stays set after MX_TIM1_Init and it locks my flash for any operation.Did anybody saw this kind of problem?Any help will be appreciate...
Hi, I would like to use USART1 insted of LPUART1 on LoRaWAN_AT_Slave exmaple. But when I try to do this, I can't choose USART1 on Middleware->LORAWAN->VCOM parameter in STMCubeMX (see screenshot).I don't understand why, thus in LoRaWAN_End_Node, it i...
Hi.I tried to use TAG_OTA_END and TAG_OTA_START from BLE_HeartRate_ota ST project the same it is used in this project to verify the FOTA operation was finished successfully.I added both, PLACE_IN_SECTION in my ble file and also I added this tags in t...
Hi, I have a problem with USB CDC on STM32WB55CE,My Project version is v1.13.& ble stack(stm32wb5x_BLE_Stack_basic_fw V1.15.0)it's all good on WB55CG(1M)but when I use WB55CE(512K)my CDC can work with no ble stack,and it will failure with stack, My c...
I get the following error when I attempt to Build or Clean any project.21:36:49 **** Build of configuration Debug for project BLE_HeartRate **** make -j12 all "make -j12 all" terminated with exit code -1073741515. Build might be incomplete. 21:36:...
Hy, I'm currently working on a project that requires CAN and that information needs to be sent via wireless, for that reason, I chose the NUCLEO stm32WL board. To make the CAN work I have to use the MCP2515 module, that converts CAN to SPI so that th...