STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

What is the device behavior when operating near the maximum junction temperature? Specifically what is/are the failure mode(s)? Leakage current? Latch-up? Die melt?

Have an application for STM32WB55 which is likely to be occasionally exposed to 125C (max) ambient, but with very low power consumption. What is the behavior at the allowed limit? Do leakage currents increase dramatically (leading to thermal runawa...

KHepp.1 by Associate
  • 1404 Views
  • 2 replies
  • 0 kudos

Writing to address 0 prevents from entering shutdown mode

If I write to address 0, it prevents from entering shutdown mode.The vector table is relocated to code.As far as I understand, writing to address 0 in this case is not illegal. For sure it does not generates a fault.The following code enters shutdown...

HugoL by Associate II
  • 1235 Views
  • 1 replies
  • 1 kudos