NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello,I am playing with NUCLEO-WB15CC board + zephyr + BLE beacon example. After compiling and flashing the example to the board I got "Precise data bus error" during Bluetooth initialization.Because zephyr does not support stm32wb15 out of the box, ...
BLE-HID demo of STM32Cube_FW_WB_V1.14.1 not working with Android 13 ?Hello,The BLE_Hid of demo STM32Cube_FW_WB_V1.14.1 does not work with my Android 13 phone at all (services cannot be listed at all in nRFconnect)while it only kind of works with my A...
We have 2 devices on one I2C port. We require fast DMA RX for high data throughput. We use circular buffers to shadow the FIFO on each device. We do this all the time with one I2C device. Two devices on the same I2C line seems impossible using the ST...
Hi allI am trying to test and implement a multicast LoRa network using the STM32WL.I have been going through the thread: https://community.st.com/s/question/0D53W00001JCdeESAT/has-anyone-managed-to-make-a-working-lorawan-multicast-with-stm32wl-if-so-...
I am trying to use as little power as possible, I want my board to wake up every 30 seconds or so, check if battery has been sufficiently charged, if not, go back to sleep, if it has then turn off rtc and do a function. Is it possible to disable rtc ...
Hi Team,I'm using STM32WLE5 MUC for Lora communication (SubGHz_Phy), I want to know is there a way to use Systick instead of timer ?This is because I used RTC to some other use case. kindly share me the way for the same.Thanks,
In STM32WB55 the LSF must be 32KHz or it can be others like 42KHz etc. as well? Thanks.
I want to know maximun number of pairing device information can the STM32WB save.Is regard to device's flash capacity?
Kind folks,STM32Cube IDE newbie here, so please forgive the simple questions.Context:I'm trying to create a multi-vendor testbed and diagnostic environment for Matter networks. In the case of ST Micro products, the thought occurs that the two Thread...