STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 161 Views
  • 0 replies
  • 0 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4035 Views
  • 0 replies
  • 3 kudos

Resolved! implementing Nucleo Board examples in DK board

Hi I am new to the WBA series and am currently working with STM32WBA55G-DK1 board to implement the audio examples.I have a doubt, Can I implement my own custom profiles for sensor data transfer along with the audio, so that, when connected to an app,...

Pallavi by Associate III
  • 2222 Views
  • 4 replies
  • 3 kudos

Resolved! Nucleo-WBA52CG issue after hard reset

Hi, I have a NUCLEO-WBA52CG dev board.I am seeing an issue whenever I do hard reset for the first time after power-on.After power-on my the loaded application works as expected, after a hard reset(using the button), the clock configuration seems to b...

Resolved! NUCLEO-WB55RG with BLE_HID_Mouse example not connecting.

After flashing NUCLEO-WB55RG board with the executable file from BLE_HID_Mouse examplecan't pair the board with the BLE of a computer. Add a device - does not see it!I have LMP 11.2292 - Bluetooth 5.2What should I do?Also, in BLE_HID mouse example RE...

GS2 by Senior II
  • 2795 Views
  • 5 replies
  • 2 kudos

STM32WL with RGB, TIM16, PWM & DMA

Hello Everyone, I'm driving the WS2812 RGB-LED using TIM16 CH1.I have a very similar behavior as in this_post . The RGB works well just until MX_LoRaWAN_Process(void) then it doesn't work. I tried his solution but it didn't work(although I suspect th...

AElgh_1-1706290666482.png
AElgh by Associate III
  • 2437 Views
  • 3 replies
  • 0 kudos

Resolved! Audio example in Nucleo-WBA55CG

Hi @STTwo-32  @TDK @KDJEM.1 @Issamos @Remy ISSALYS ,I have started using Nucleo-WBA55CG for BLE Audio and realized STM32Cube_FW_WBA_V1.3.0 does not contain any audio code for the board. But STM32WBA55CG- DK1 has the ble audio snippet code.Can I use t...

Pallavi by Associate III
  • 3426 Views
  • 6 replies
  • 2 kudos

Resolved! Custom Template BLE and LPM

I everyone ,I'm working on a STM32WB35I've build a small custom server app with just a simple batt level service it works and advertise perfectly if I don't enable LPM as soon as I enable LPM it don't advertise anymoreit looks as if CPU2 and RF are d...

oga_0-1712761048851.png oga_1-1712761081244.png oga_0-1712829155087.png
oga by Associate III
  • 2383 Views
  • 4 replies
  • 0 kudos