User Activity

Hello,We have an issue with the B-WL5M-SUBG1 evaluation board: The idle current consumption is higher than expected: 89 uA (vs. expected: 1-2 uA) after joining (OTAA) successfully.Board: B-WL5M-SUBG1Firmware: STM32CubeWL/Projects/B-WL5M-SUBG1/Applica...
Hi, The font size is way too small for me. I use Ubuntu, system-wide font scaling factor set to 1.5. This does not affect the font in STM32CubeMonitor. It is really small. Any ideas how the font size can be increased? STM32CubeMonitor-Power - v1.2.1 ...
STM32CubeWL = "STM32Cube MCU Package for STM32WL series", currently version 1.3.0.Is there a new release planned?Background: We are using version 1.3.0. We have issues with an application based on LoRaWAN_End_Node_FreeRTOS. We suspect the FreeRTOS in...
Hi all,We have a sporadic issue which is difficult to debug. Maybe you can give some advice / solutions / hints? Any input is welcome!We are working on an application based on the project LoRaWAN_End_Node_FreeRTOS of STM32CubeWL V1.3.0, board: Nucleo...
Hello community,We are using STM32WL V1.2.0 to develop an application based on the example application "LoRaWAN_End_Node_FreeRTOS". Board: Nucleo-WL55JC1. The example application works.However, as soon as we add the function "osDelay(2000)" in a thre...
Kudos from
Kudos given to