STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

Resolved! BLE with audio and signal processing

Hi,I am looking for a MCU with BLE5 and audio. If BLE5 is not available with audio, then I will get compromised with Classic bluetooth. If such an MCU has signal processing capability then it will be an added advantage for me, so that I will not use ...

Resolved! P-NUCLEO-LRWAN2 - gateway firmware sources

 Hello,The firmware for the P-NUCLEO-LRWAN2 gateway is currently provided as a binary file named "st-nucleo-lora-gw-at-fw-v2.1.7-eu868-TTN.bin." I am very interested in obtaining access to the source code to develop a modified version of the firmware...

Resolved! implementing Nucleo Board examples in DK board

Hi I am new to the WBA series and am currently working with STM32WBA55G-DK1 board to implement the audio examples.I have a doubt, Can I implement my own custom profiles for sensor data transfer along with the audio, so that, when connected to an app,...

Pallavi by Associate III
  • 2254 Views
  • 4 replies
  • 3 kudos

Resolved! Nucleo-WBA52CG issue after hard reset

Hi, I have a NUCLEO-WBA52CG dev board.I am seeing an issue whenever I do hard reset for the first time after power-on.After power-on my the loaded application works as expected, after a hard reset(using the button), the clock configuration seems to b...

Resolved! NUCLEO-WB55RG with BLE_HID_Mouse example not connecting.

After flashing NUCLEO-WB55RG board with the executable file from BLE_HID_Mouse examplecan't pair the board with the BLE of a computer. Add a device - does not see it!I have LMP 11.2292 - Bluetooth 5.2What should I do?Also, in BLE_HID mouse example RE...

GS2 by Senior II
  • 2825 Views
  • 5 replies
  • 2 kudos