NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello, I am following this tutorial, but it is designed for the WB55 and I am using the WB15. I have managed to get the LED task before this one working. However with this task I do not get an output to the App. I have modified the code to have an LE...
Hello, I hope you are doing well.I’ve developed a product using the STM32H573I-DK kit as a reference and the MXCHIP EMW3080 Wi-Fi module. We decided to design our new hardware in such a way that the Wi-Fi module could be connected just like in the de...
Hi ST Community Is it possible to use the ADC polling/DMA/IT in STOP2 mode. The application is to develop a low power platform for ADC sampling and go back to sleep. After a certain period send this data over BLE.
・OverviewThis project involves the development of Matter devices. We encountered an issue with commissioning the device using the obtained vendor ID. Despite following the necessary steps, the commissioning process fails. Below, we detail the steps t...
Hello,I am working on an STM32WB project where I need to erase and write to the flash memory. I have utilized the flash_driver.c files that I found in the STM32WB examples. I tried to integrate these into my project (which does not use FreeRTOS or BL...
Hi,Are there any plans for a such a module in the near future? (preferable also with combined BLE-support)If so, what approx. timeline?Thanks
Is it possible to use stm32wb55 radio without DLF162500? I mean I have nothing to complain about its price but rather that it uses a non standard package/footprint and I don't want to have any non standard components so I can change components so lon...
When using the radio for bluetooth, would it really make a huge difference in power consumption? I want to reduce my bom and would much rather not depend on 2 more inductors, also is the 32khz really that necessary?
Had tried for some time but still did not get it. The MCU and sensor are both mainstream, typical and relatively simple.Any pointer to a complete (with STM32 project and MX .ioc) example code for STM32 MCU SPI interfacing with a sensor chip. Many t...
Dear community,I recently faced a possible anomaly in Stm32 cube configuration when setting up the RTC alarm:the rtc alarm interrupt was firing immediatley during initialization.Everything was setup via Cube, no manual code involved.Problem begins im...