STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

BLE extended advertising parsing

  Hello Team ST, I am currently working on parsing my extended BLE data using the BLE_p2pClient_Ext application, specifically the `analyse_ext_adv_report` function to view the advertising data. However, I am having trouble parsing and appending the f...

Hardik02 by Associate II
  • 1548 Views
  • 2 replies
  • 0 kudos

STM32WB Low Power mode

Here's a revised version of your message:---Hi,I am using the NUCLEO-WB15CC board for a custom application where I read an analog sensor value with a 12-bit ADC resolution. The issue arises when I try to transmit this data over BLE. I am using the fo...

STM32WL5Mo dosent respond to ST-LINK

Hello,I'm trying to connect my ST-LINK-PWR V3 to my own bord with a STM32WL5M0 but it doesn't wrok. I also tried with a J-Link probe and a Nucleo board and that doesn't work either.I modified my card to work at 3.3V, no improvement.The MCU is fresh f...

laesser_0-1729496289715.png
laesser by Associate II
  • 1174 Views
  • 1 replies
  • 0 kudos

STM32WB09: Cannot build BLE project

I cannot build a simple BLE project using the newest version of STM32CUBEIDE (1.16.1) for the STM32WB09KE.Steps taken:Create new project for the STM32WB09KE.Enable all dependencies needed for RADIO, RADIO_TIMER and STM32_BLE, and enabled those.When t...

s215477 by Associate II
  • 2627 Views
  • 4 replies
  • 1 kudos

Resolved! Matching network for antenna design for STM32WL33

Hello,While using a unit as a receiver module, is the matching network required for the Tx pins as well?Also, since there is no data being transmitted, how should the VFBSD pin (power pin for the RF section) be connected in this case?Regards,Leah 

query.png