Skip to main content
APort
Associate III
Mar 20, 2024 9:00 AM UTC
Solved

aci_gatt_update_char_value_ext issue

Hello,

We are trying to use MTU larger than 24X bytes.

The characteristic size set to 483 bytes (CFG_BLE_MAX_ATT_MTU).

We tried to use aci_gatt_update_char_value_ext to set the value (as the HCI layer is limited to 255 bytes transfer).

aci_gatt_update_char_value_ext called twice (for both MPSs) , first part with 0 offset, and 2nd with 240.

First, Update_Type=GATT_CHAR_UPDATE_LOCAL_ONLY;  2nd call with GATT_CHAR_UPDATE_SEND_NOTIFICATION.

What happens is that random? number of bytes is sent (80).

 

If we always use GATT_CHAR_UPDATE_SEND_NOTIFICATION proper 480 bytes are sent, but twice (for both offset updates) ...

 

Thanks in advance

 

 

This topic has been closed for replies.
STTwo-32
STTwo-32Best answer
ST Technical Moderator
May 23, 2024 7:00 AM UTC

Hello @APort 

What I understand, you are looking to send more data. So, I suggest you refer to this description:

1. Modify CFG_BLE_MAX_ATT_MTU to 512 in app_conf.h

2. Call aci_gatt_exchange_config() after connecting in app_ble.c:

tBleStatus status = aci_gatt_exchange_config(BleApplicationContext.BleApplicationContext_legacy.connectionHandle);

 3. Change Notify characteristic size in p2p_stm.c: 

aci_gatt_add_char(aPeerToPeerContext.PeerToPeerSvcHdle, UUID_TYPE_128, &uuid16,
 CFG_BLE_MAX_ATT_MTU - 3, // [STM]
 CHAR_PROP_NOTIFY, ATTR_PERMISSION_NONE,
 GATT_NOTIFY_ATTRIBUTE_WRITE, /* gattEvtMask */
 10, /* encryKeySize */
 1, /* isVariable: 1 */
 &(aPeerToPeerContext.P2PNotifyServerToClientCharHdle));

4. Change P2PS_STM_App_Update_Char function in p2p_stm.c:

tBleStatus P2PS_STM_App_Update_Char(uint16_t UUID, uint8_t *pPayload) 
{
 tBleStatus result = BLE_STATUS_INVALID_PARAMS;
 switch(UUID)
 {
 case P2P_NOTIFY_CHAR_UUID:
 
 aci_gatt_update_char_value_ext(0x0000,
 aPeerToPeerContext.PeerToPeerSvcHdle,
 aPeerToPeerContext.P2PNotifyServerToClientCharHdle,
 0x00,
 509,
 0,
 243,
 (uint8_t *) pPayload);
 

 aci_gatt_update_char_value_ext(0x0000,
 aPeerToPeerContext.PeerToPeerSvcHdle,
 aPeerToPeerContext.P2PNotifyServerToClientCharHdle,
 0x00,
 509,
 243,
 243,
 (uint8_t *) pPayload + 243);
 
 aci_gatt_update_char_value_ext(0x0000,
 aPeerToPeerContext.PeerToPeerSvcHdle,
 aPeerToPeerContext.P2PNotifyServerToClientCharHdle,
 0x01,
 509,
 486,
 23,
 (uint8_t *) pPayload + 486); 

 break;

 default:
 break;
 }

 return result;
}

5. Modify P2PS_STM_Data_t structure in p2p_stm.h:

typedef struct
{
 uint8_t * pPayload;
 uint16_t Length;
}P2PS_STM_Data_t; 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

STTwo-32
STTwo-32Best answer
ST Technical Moderator
May 23, 2024 7:00 AM UTC

Hello @APort 

What I understand, you are looking to send more data. So, I suggest you refer to this description:

1. Modify CFG_BLE_MAX_ATT_MTU to 512 in app_conf.h

2. Call aci_gatt_exchange_config() after connecting in app_ble.c:

tBleStatus status = aci_gatt_exchange_config(BleApplicationContext.BleApplicationContext_legacy.connectionHandle);

 3. Change Notify characteristic size in p2p_stm.c: 

aci_gatt_add_char(aPeerToPeerContext.PeerToPeerSvcHdle, UUID_TYPE_128, &uuid16,
 CFG_BLE_MAX_ATT_MTU - 3, // [STM]
 CHAR_PROP_NOTIFY, ATTR_PERMISSION_NONE,
 GATT_NOTIFY_ATTRIBUTE_WRITE, /* gattEvtMask */
 10, /* encryKeySize */
 1, /* isVariable: 1 */
 &(aPeerToPeerContext.P2PNotifyServerToClientCharHdle));

4. Change P2PS_STM_App_Update_Char function in p2p_stm.c:

tBleStatus P2PS_STM_App_Update_Char(uint16_t UUID, uint8_t *pPayload) 
{
 tBleStatus result = BLE_STATUS_INVALID_PARAMS;
 switch(UUID)
 {
 case P2P_NOTIFY_CHAR_UUID:
 
 aci_gatt_update_char_value_ext(0x0000,
 aPeerToPeerContext.PeerToPeerSvcHdle,
 aPeerToPeerContext.P2PNotifyServerToClientCharHdle,
 0x00,
 509,
 0,
 243,
 (uint8_t *) pPayload);
 

 aci_gatt_update_char_value_ext(0x0000,
 aPeerToPeerContext.PeerToPeerSvcHdle,
 aPeerToPeerContext.P2PNotifyServerToClientCharHdle,
 0x00,
 509,
 243,
 243,
 (uint8_t *) pPayload + 243);
 
 aci_gatt_update_char_value_ext(0x0000,
 aPeerToPeerContext.PeerToPeerSvcHdle,
 aPeerToPeerContext.P2PNotifyServerToClientCharHdle,
 0x01,
 509,
 486,
 23,
 (uint8_t *) pPayload + 486); 

 break;

 default:
 break;
 }

 return result;
}

5. Modify P2PS_STM_Data_t structure in p2p_stm.h:

typedef struct
{
 uint8_t * pPayload;
 uint16_t Length;
}P2PS_STM_Data_t; 

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.