STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

STM32WL Maximum storage temperature

I have an unusual question. The storage temperature range for an STM32WL is stated as: -65 to +150 °C.We are looking at doing some particular tests at high temperatures for radiation exposure recovery, so some questions if anyone knows:1. If we put t...

Resolved! Wake up MCU from STOP2 mode

HelloWe are working on a product using the STM32WLE5JC MCU. The features a magnetic switch that generates interrupts (specifically a low to high transition) which is meant to wake up the MCU from STOP2 mode. What is the ideal way to do this? We have ...

Resolved! BLE Advertising raw data

Hi,I am currently playing with the NUCLEO-WBA55 board with the BLE_p2pServer_ota example.During the advertising process, I got this raw data with the BLE scanner on my phone. I mean that the 0x30 is the ID for STMicroelectronics, but what is behind i...

2024-10-30_12h50_35.png
ledi001 by Senior
  • 1845 Views
  • 1 replies
  • 1 kudos

Resolved! how to enable uart interrupt

Hello,I want to activate UART1 interrupt directly through code in STM32CubeIDE, without using the .ioc file. UART1 is already active, so I just need to add the necessary lines to enable the interrupt.In the stm32wbxx_it.c file, I defined the interrup...

Ndemir by Associate II
  • 4985 Views
  • 4 replies
  • 0 kudos

Resolved! STM32WLE5JCI6 RX Sensitivty

Hi , is it possible to get the RX sensitivity of the STM32WLE5JCI6 in other LORA conditions then mentioned in the Datasheet ? our LORA parameters are:PER=1%BW= 20.8Khz to 125KhzSF= 7  to 11split RF paths for RX and TX using RF SWITCH Thank you,Viola

viola by Associate III
  • 1104 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WB55: Zigbee Reporting OnOff Server Attribute

Hello,I am trying to use WB55 as a Zigbee device on HomeAssistant. I have made some progress so far, and I can use it as an OnOff switch on HomeAssistant and report my switch status in real-time to HomeAssistant.At first, I added WB55 to HomeAssistan...

DL_Weng by Associate II
  • 6576 Views
  • 7 replies
  • 0 kudos

BLE Scan Filter

Hi ST CommunityI'm working on a BLE Beacon application. There is a device which is beaconing every second. Goal is to scan for these beacons and update to gateway.  Using this function 'aci_gap_start_general_discovery_proc' to scan for the beaconing ...

ABN by Associate III
  • 1065 Views
  • 0 replies
  • 0 kudos

STM32WLE5 subGhz Frequency offset vs supply voltage drop

Hi ,In table 32 in the Datasheet we can see TXDRP parameter which describes RF output power drop versus supply voltage. is there also RF frequency offset as a result of the supply voltage drop ? If the answer is yes - can you estimate it ? Thank you,...

viola by Associate III
  • 2182 Views
  • 4 replies
  • 0 kudos