STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

Resolved! BLE_ZIGBEE_RFD_Dynamic consumption testing report

Testing Background:The current device requirements are as follows:It should operate in low-power Bluetooth mode as a BLE controller (only running the Bluetooth protocol).It should be able to run both the Zigbee and Bluetooth protocols simultaneously ...

DL_Weng_0-1731059960113.png DL_Weng_1-1731059960151.png DL_Weng_2-1731059960158.png DL_Weng_3-1731059960201.png
DL_Weng by Associate II
  • 1596 Views
  • 1 replies
  • 0 kudos

STM32WB5mmdk standby mode

In my ble application(BLE peripheral) code i need to enter standby mode(BLE can be disabled in stand by mode), after 20 sec by RTC wake up i need to enable the BLE again, start advertising and do some ADC reading. Is there any particular example code...

samuel_l by Associate II
  • 3598 Views
  • 8 replies
  • 1 kudos

Resolved! Tx radio power on STM32 Nucleo WBA55CG using Zephyr

Hi, I am using the STM32 Nucleo WBA52CG evaluation board and programming it using Zephyr v3.7.0 and am looking how to set the Tx output power of the BLE radio. Are there any configs available in Zephyr for the same?  If not, alternatively please sugg...

BKaiwalya by Associate II
  • 4370 Views
  • 7 replies
  • 0 kudos

Resolved! Green Power Device cluster missing in CubeMX ?

Hello,I'm currently working with the STM32WB55 evaluation card (P-Nucleo WB55). According to the data sheet, those MCUs supports ZigBee 3.0 which include Green Power configuration.However, I can't seem to find the Green Power Device (End device) clus...

CMiqu.1 by Associate II
  • 2917 Views
  • 6 replies
  • 1 kudos

stm32WB5MM Matter/Thread commissioning failing

Hi Setup and IssueI am struggling to get my stm32WB5MM running the light application to commission on my Rasperberry pi4 (Ubuntu 24.04.1 LTS) with the openthread-border-router and chip-tool installed with snap (edge version to be compatible with the ...

mpsbrandt_0-1730887988269.png