STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

Resolved! cannot use NVIC_SetVector

I am trying to write interrupts bare-metal style. When I try to set the interrupt vector for LPTIM1 (using B-L071Z-LRWAN1) using this method, NVIC_SetVector(LPTIM1_IRQn, (uint32_t)&LPTIM1_IRQHandler); the compiler gives me this error:../Core/Src/main...

STM32Wb09 ACI or HCI communication with Host MCU

Hello ST,For our project, we would like to use STM32WB09KE chip as a Bluetooth MCU and would like to establish communication with the HOST MCU ex:- Stm32H5.Do you have any protocol, how we can make communication both ways from the Main MCU to enable ...

teja_111 by Associate II
  • 1561 Views
  • 1 replies
  • 1 kudos

Resolved! RTC and Timer Issues with BLE Stack on STM32WB35CEU6A

Hello,When I add the BLE stack to the STM32WB35CEU6A, I notice that the RTC and timer settings don’t work correctly. With the BLE stack enabled, I can’t get accurate time information from the RTC and timer, or there are inconsistencies in the timing....

Resolved! Request for Hardware design guide for STM32WL33

Hello, I'm a beginner in hardware design for STM32 MCU wireless. I usually get detailed information about component value recommendations in the datasheet or application note. But in STM32WL33, I get unclearer information than in other MCU wireless d...

gusti_made_0-1730433815741.png

Resolved! Flash Memory Configuration in STM32WB55RGV6

I am currently working with the STM32WB55RGV6 microcontroller, which has a total of 1 MB of Flash memory. However, after generating a project using STM32CubeMX, I noticed that the Flash memory file only indicates 512 KB of available memory.Could you ...

Smalik by Associate II
  • 2601 Views
  • 5 replies
  • 0 kudos

Resolved! How to connect NUCLEO STM32WB55 onboard programmer to STM32F411 board ?

Hello,Does anybody knows - are 4 wires enough for programming: STM32F411CEU6 module      JP5 of the NUCLEO-WB55RGGND                                        <---- T_VDDSWSCK                                    ??? SWOSWDIO                              ...

GS2 by Senior II
  • 2210 Views
  • 3 replies
  • 0 kudos

Set RTC without resetting HW timer server?

My STM32WB5MMG application interfaces with a GPS receiver. Ideally, what I would like to do is to update the RTC date/time every time I get a timepulse signal from the GPS, so that the RTC date/time is always as close as possible to GPS time. However...

crwper by Senior
  • 1127 Views
  • 0 replies
  • 0 kudos

Resolved! stm32wl33

Hello, Iam trying look for low budget chip for my application, Can you guide if stm32wl33 will work for lorawan communication to send temp. data