STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 220 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

Resolved! Zigbee Green Power Proxy with STM32WB55

I wonder, if it is possible to build a Zigbee Green Power Proxy and ZGP Sink with the STM32_WPAN v1.0.I couldn't find any documentation neither any source code samples.I did find some hints about Zigbee Green Power:1. https://wiki.st.com/stm32mcu/wik...

Bildschirmfoto 2024-11-11 um 11.37.49.png Bildschirmfoto 2024-11-11 um 11.41.48.png
aritec by Associate III
  • 1938 Views
  • 2 replies
  • 1 kudos

STM32WB15 BLE OTA Custom Application Never Boots

I am building an application which needs to be updated over BLE OTA.  I have followed the getting started videos and AN5247.  I have flashed the BLE_Ota example to address 0x0800 0000 as instructed, and I can successfully connect to the device using ...

ironduck_0-1731443257728.png ironduck_1-1731443361837.png ironduck_2-1731443522168.png
ironduck by Associate
  • 1032 Views
  • 1 replies
  • 0 kudos

STM32WLE5 Power Amp Fails

Hello, First Post here.I have been testing 20 prototype STM32WLE5 boards and have been getting a respectable +20dBm output power at 908 MHz Lora Modulation 125KHz BW drawing 105mA.  VR_PA = 2.5V. This is great!However, on two of the boards the RFO_HP...

buba049 by Associate
  • 1606 Views
  • 2 replies
  • 1 kudos

Resolved! STM32WBA52xx - SCAN_RSP

Hello, im trying to sending manufacturer-specific data using the SCAN_RSP AdvData in the BLE_p2pServer_Ext application on the STM32WBA module. Are there any examples? Thank You.

MLiska by Associate II
  • 921 Views
  • 1 replies
  • 0 kudos

Reducing BLE scan time in STM32WBMMG

Hello,In my project, the initial Bluetooth scanning time(I am using STM32WB5MMG) takes 10 seconds (gap discovery procedure). Is it possible to reduce this to 5 seconds or less? Although I have adjusted the scan interval and scan window values, they d...