NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello,i try to program LSM100A ( STM32WLE5CC ) .i can connect but can't program an elf file : error fail to erase memory, then cube programmer crashed.thank you for supportlogs :## A fatal error has been detected by the Java Runtime Environment:## SI...
Hi, I am building a BLE application using Zephyr v3.7.0 and nucleo_wba55cg evaluation board. I have currently implemented the accept list functionality where only paired and bonded devices can connect in accept list adv mode. However, I struggle with...
Hi,We are encountering a problem with an STM32WB55-based Zigbee router we have developed, where, in some cases, the Zigbee end device connected via the router becomes unreachable for requests sent from the coordinator.Specifically, when the STM32WB55...
Hello,I am currently working with the NUCLEO-WL33CC1 boards (MB2029-HIGHBAND-B02 + MB1801D). I have successfully ported our wireless solution to this platform (6tisch stack). Transceiver works properly, no problems so far.However, my next step is to ...
Hi,How can I set the lowest power consumption with the BLE_p2pServer example on the STM32WBA55?I have tried to set the power level to the lowest level in STM32_WPAN configuration,but the average power consumption (at 2s advertising interval) is aroun...
Hello,we are tryng implemet wmbus in our meter.is ther any example code availble for it.I am usng stm32wle5ccu6. if any have done it let me know. thank you.
Hello,My goal is to setup a timer which also runs when the device is in (Zigbee) sleep mode. I have tried to adapt HAL_GetTick() to be run by LPTIM1 on an STM32WB5MMG, which led to the device not boot anymore. I also tried setup timestamps on the RTC...
Hi,after flashing the binary files of BLE_ApplicationInstallManager and BLE_p2pServer_ota on the STM32WBA55CG, I can no longer access the controller.What i did:Flashing .bin file of the BLE_ApplicationInstallManager @ start address 0x0800 0000Flashin...
Hi,I am looking for wireless solution which supports below protocols.1> LoRaWAN.2> Sigfox3> WMbus.I am also looking for firmware integration for all of the above protocols and need to find that the firmware will support all of the protocols at same t...
STM32WB5MMG datasheet says ANT_NC should be connected to no-connect pad on board. But then, example ground plane seems to connect to ANT_NC. Which is right?