STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

low power mode using touchGFX

Hi,I am using STM32F469I-DISCO with touchGFX on it, and I would like to reduce power consumption. I managed to set the brightness of LCD to lowest when no user activity for more than 30sec.I am resetting brightness as soon as the user touch the scree...

Resolved! Progress Widgets with transparent background

Hi all,For my GUI I need several circle and box progress widgets in different sizes that have a transparent background, e.g. only showing the actual progress "line" and nothing else. So far I achieved this by simply choosing a transparent PNG as back...

SaschaK by Associate II
  • 2835 Views
  • 6 replies
  • 1 kudos

Resolved! Text Area Widgets in Touchgfx

Hello!This is written that Touchgfx widget 'Text Area' if has enabled the action 'WIDE_TEXT_WORDWRAP' then the call 'getTextWidth()' will return the width of the widest line but it returns the width of the total text area.Can you please check how to ...

Hafsa by Associate
  • 1749 Views
  • 4 replies
  • 0 kudos

Resolved! No image on LCD screen in touchgfx

 Hi ! I am using MT25Q128 on LCD screen with stm32f746 and the image comes out fine.If I use MT25Q128 instead of MT25Q256 in memory, the image is not displayed.The program modification is modified for MT25Q256 in Driver->BSP->stm32746g_discovery_qspi...

Why isn't there a dropbox list widget?

I need a dropbox list widget and can't seem to find one in the toolkit.1. Are there 3rd party vendors that offer this or other UI elements?2. Can the existing widgets be assembled to implement a dropdown list widget?  If so, can you please explain th...