Skip to main content
Associate
November 2, 2024
Question

Unable to LTDC ReConfigure/Reinit after LTDC Deinit

  • November 2, 2024
  • 7 replies
  • 1795 views
 
Hi,

I am trying to reinitialize the LTDC-TFT LCD controller in a task when I press a button.

I am using the STM32H735G-DK kit, which has a TFT LCD. I have created a project using TouchGFX, and it seems the display gets initialized and loaded with images from the TouchGFX init and TouchGFX task.

Firstly, I want to achieve the re-initialization of the LTDC-TFT LCD on the STM32H735G-DK.
when i try re initializing the LTDC, it got freeze, not sure how to unfreeze it, display goes blank unable to restore back all the images which has been loaded after a reset

I am working on the low-power modes of the STM32H735G-DK and want to make sure the display goes off when I put the controller in sleep/stop mode and wakes up along with other peripherals after an external wake-up signal.

rakesh1_0-1730545920340.png
Above image which states LTDC has the 4 power modes, one of it is STOP mode
if LTDC Got freeze in STOP mode, how to unfreeze it?
can we make it work in stop mode? if yes how can we reconfigure the LTDC?

Here is what I have tried:

void test_task(void)
{
for(;;)
{

if (Button_Pressed ==1)

{

Button_Pressed=0;

printf("Entering sleep mode...\n");

HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);

SystemClock_Config();

vDisplay_Reinit();

printf("\n\r Exiting sleep mode\n\r");

}
}
}

void vDisplay_Reinit(void)
{
HAL_LTDC_MspDeInit(&hltdc);
HAL_DMA2D_MspDeInit(&hdma2d);

osDelay(10);

HAL_Init();
MX_GPIO_Init();
MX_DMA2D_Init();
MX_LTDC_Init();
MX_OCTOSPI1_Init();
MX_OCTOSPI2_Init();
MX_LIBJPEG_Init();
MX_TouchGFX_Init();
TouchGFX_Task(NULL);
}
I am able to turn the LTDC display ON & OFF using the following code:
void DisplayONOFF(void)
{

__HAL_LTDC_DISABLE(&hltdc);

/* Assert display enable LCD_DISP pin */
HAL_GPIO_WritePin(LCD_DISP_GPIO_Port, LCD_DISP_Pin, GPIO_PIN_RESET);

/* Assert backlight LCD_BL_CTRL pin */
HAL_GPIO_WritePin(LCD_BL_CTRL_GPIO_Port, LCD_BL_CTRL_Pin, GPIO_PIN_RESET);

osDelay(10);

__HAL_LTDC_ENABLE(&hltdc);

// Reset Control Pins
/* Assert display enable LCD_DISP pin */
HAL_GPIO_WritePin(LCD_DISP_GPIO_Port, LCD_DISP_Pin, GPIO_PIN_SET);

/* Assert backlight LCD_BL_CTRL pin */
HAL_GPIO_WritePin(LCD_BL_CTRL_GPIO_Port, LCD_BL_CTRL_Pin, GPIO_PIN_SET);

osDelay(10);

}

Reference Links:
STM32H7-LTDC: STM32H7-Peripheral-LCD_TFT_Controller (LTDC)
STM32H7-LTDC_AppNote: app_note 

This topic has been closed for replies.

7 replies

ST Technical Moderator
November 8, 2024

Hello Rakesh.

According to the datasheet and the table you have attached, the content of the registers are retained when using stop mode. Therefore, you shouldn't have to reinitialize the LTDC peripheral when exiting stop mode. To exit stop mode, the following is stated in the HAL_PWR driver:
(+) Exit: Any EXTI Line (Internal or External) configured in Interrupt/Event mode.

So any interrupt will exit stop mode.

Regarding your other question on how to reconfigure the LTDC, could you share the content of your HAL_LTDC_MspDeInit() function? Are you sure you couldn't just use the HAL_LTDC_DeInit() function? The same goes for DMA2D.


Best regards,
Johan
rakesh1Author
Associate
November 11, 2024

Hello Johan,

Thanks for your reply,
I have tried to reinitialize the Display Using
HAL_LTDC_DeInit(&hltdc) & HAL_DMA2D_DeInit(&hdma2d) functions, but these couldn't help me to bring back the display after wakeup from the stop mode...so that's why I have tried using HAL_LTDC_MspDeInit functions

I'll make a brief about my goal, I wanted to bring up the display after wakeup from the stop mode, in the freeRTOS (CMISI V2.0) environment, the Touch gfx task wasn't running correctly as expected after wakeup, and the display was not loading with the images after wakeup which as earlier(before entering into stop mode)

I have attached the Project which I'm working on, it has been created using touch gfx, and PC13 (EXTI) was used to wake up the source ( USER BUTTON on STM32H735GDK)

now I have implemented a system that goes to stop mode, and when I press the user button wakes the system, the process repeats,
continue the other tasks where all stopped after wakeup, and reload the all images and fonts, UI content in Display using touch gfx( which is not happening in my case)

Could you please check out the same!!, ignore me if any mistakes are made!

Please let me know what sequence/steps are missed, Is there any specific sequence after wakeup and before going to stop mode, to continue from where does it stop?

I have tried to check the RTC wakeup example: Example:https://github.com/STMicroelectronics/STM32CubeH7/tree/master/Projects/STM32H735G-DK/Examples/PWR/PWR_STOP_RTC 

 

FYI, HAL_LTDC_MspDeInit,HAL_DMA2D_MspInit functions 
/**
* @brief LTDC MSP De-Initialization
* This function freeze the hardware resources used in this example
* hltdc: LTDC handle pointer
* @retval None
*/
void HAL_LTDC_MspDeInit(LTDC_HandleTypeDef* hltdc)
{
 if(hltdc->Instance==LTDC)
 {
 /* USER CODE BEGIN LTDC_MspDeInit 0 */

 /* USER CODE END LTDC_MspDeInit 0 */
 /* Peripheral clock disable */
 __HAL_RCC_LTDC_CLK_DISABLE();

 /**LTDC GPIO Configuration
 PB8 ------> LTDC_B6
 PD3 ------> LTDC_G7
 PB9 ------> LTDC_B7
 PE0 ------> LTDC_R0
 PA8 ------> LTDC_B3
 PE1 ------> LTDC_R6
 PG14 ------> LTDC_B0
 PD0 ------> LTDC_B1
 PD6 ------> LTDC_B2
 PH15 ------> LTDC_G4
 PC7 ------> LTDC_G6
 PC6 ------> LTDC_HSYNC
 PG7 ------> LTDC_CLK
 PB1 ------> LTDC_G0
 PH11 ------> LTDC_R5
 PH9 ------> LTDC_R3
 PA3 ------> LTDC_B5
 PH8 ------> LTDC_R2
 PH10 ------> LTDC_R4
 PH4 ------> LTDC_G5
 PA4 ------> LTDC_VSYNC
 PE12 ------> LTDC_B4
 PE13 ------> LTDC_DE
 PE15 ------> LTDC_R7
 PH3 ------> LTDC_R1
 PA6 ------> LTDC_G2
 PB0 ------> LTDC_G1
 PE11 ------> LTDC_G3
 */
 HAL_GPIO_DeInit(GPIOB, GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_1|GPIO_PIN_0);

 HAL_GPIO_DeInit(GPIOD, GPIO_PIN_3|GPIO_PIN_0|GPIO_PIN_6);

 HAL_GPIO_DeInit(GPIOE, GPIO_PIN_0|GPIO_PIN_1|GPIO_PIN_12|GPIO_PIN_13
 |GPIO_PIN_15|GPIO_PIN_11);

 HAL_GPIO_DeInit(GPIOA, GPIO_PIN_8|GPIO_PIN_3|GPIO_PIN_4|GPIO_PIN_6);

 HAL_GPIO_DeInit(GPIOG, GPIO_PIN_14|GPIO_PIN_7);

 HAL_GPIO_DeInit(GPIOH, GPIO_PIN_15|GPIO_PIN_11|GPIO_PIN_9|GPIO_PIN_8
 |GPIO_PIN_10|GPIO_PIN_4|GPIO_PIN_3);

 HAL_GPIO_DeInit(GPIOC, GPIO_PIN_7|GPIO_PIN_6);

 /* LTDC interrupt DeInit */
 HAL_NVIC_DisableIRQ(LTDC_IRQn);
 /* USER CODE BEGIN LTDC_MspDeInit 1 */

 /* USER CODE END LTDC_MspDeInit 1 */
 }

}

/**
* @brief DMA2D MSP Initialization
* This function configures the hardware resources used in this example
* hdma2d: DMA2D handle pointer
* @retval None
*/
void HAL_DMA2D_MspInit(DMA2D_HandleTypeDef* hdma2d)
{
 if(hdma2d->Instance==DMA2D)
 {
 /* USER CODE BEGIN DMA2D_MspInit 0 */

 /* USER CODE END DMA2D_MspInit 0 */
 /* Peripheral clock enable */
 __HAL_RCC_DMA2D_CLK_ENABLE();
 /* DMA2D interrupt Init */
 HAL_NVIC_SetPriority(DMA2D_IRQn, 5, 0);
 HAL_NVIC_EnableIRQ(DMA2D_IRQn);
 /* USER CODE BEGIN DMA2D_MspInit 1 */

 /* USER CODE END DMA2D_MspInit 1 */

 }

}

 





MM..1
Super User
November 11, 2024

Locate issue and dont do reinit . LTDC too use PLL , that require restart , check if 

SystemClock_Config();

doit, when no write your code.

rakesh1Author
Associate
November 12, 2024

Hello MM,


Correct me if I'm not clear..!
I have tried removing the Display Re-initialization part after wakeup from stop mode But shows only a Blank screen, UI is not getting loaded, TouchGFX_Task() itself is not running and Other tasks are running normally(checked using prints)!

If I don't put the following line, I'm unable to see any prints and I can't visualize that other tasks are running, due to a blank screen in the display 

 

SystemClock_Config();

 

 

FYI, the sequence I have also checked Deinit LTDC, DMA2D, goto stop mode, and wakeup then Initialize the LTDC, DMA2D, OSPI, TouchGFX_Init

 

Also Tried deleting resources used by TouchGFX_Task(like Semaphores & Queues), Do I need to Delete the task and recreate the TouchGFX task to load the images/UI content?

Is there any specific sequence to be followed? If yes, please let me know the sequence to bring up the display ( loaded with UI Content/images).

<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>

if I'm not wrong you might want me to check the clock configuration, I have also tried the following clock configuration after wakeup from the stop mode, Still UI not loading correctly, but all other tasks are running except Touchgfx_Task

Are there any examples available to have an idea of how UI gets loaded after wakeup from the stop mode in STM32H735GDK?

/**
 * @brief Configures system clock after wake-up from STOP: enable HSE, PLL
 * and select PLL as system clock source.
 * @PAram None
 * @retval None
 */
static void SYSCLKConfig_STOP(void)
{
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 uint32_t pFLatency = 0;


 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
 while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}

 /* Get the Oscillators configuration according to the internal RCC registers */
 HAL_RCC_GetOscConfig(&RCC_OscInitStruct);

 /* After wake-up from STOP reconfigure the system clock: Enable HSE and PLL */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /* Get the Clocks configuration according to the internal RCC registers */
 HAL_RCC_GetClockConfig(&RCC_ClkInitStruct, &pFLatency);

 /* Select PLL as system clock source and configure the HCLK, PCLK1 and PCLK2
 clocks dividers */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, pFLatency) != HAL_OK)
 {
 Error_Handler();
 }
}

 

MM..1
Super User
November 12, 2024

I dont say remove system clock , i say about LTDC clock , that isnt init in this function. For inspire read STM32CubeH7/Projects/STM32H735G-DK/Examples/LTDC/LTDC_ColorKeying_FromOSPI/Src/stm32h7xx_hal_msp.c at master · STMicroelectronics/STM32CubeH7 · GitHub and your msp init specialy this part

 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_LTDC;
 PeriphClkInitStruct.PLL3.PLL3M = 5;
 PeriphClkInitStruct.PLL3.PLL3N = 160;
 PeriphClkInitStruct.PLL3.PLL3P = 2;
 PeriphClkInitStruct.PLL3.PLL3Q = 2;
 PeriphClkInitStruct.PLL3.PLL3R = 83;
 PeriphClkInitStruct.PLL3.PLL3FRACN = 0;
 PeriphClkInitStruct.PLL3.PLL3VCOSEL = RCC_PLL1VCOWIDE;
 PeriphClkInitStruct.PLL3.PLL3RGE = RCC_PLL1VCIRANGE_0;

 HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) ;

too RTOS require suspend task before stop etc.