STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Add chinese characters to TouchGFX fonts

When I add the unicode to the proper font for chinese characters the file gets overwritten when I generate code with TouchGFX. So how do I properly update the fonts this way in the middle of a large project?

DElli.1 by Associate III
  • 1226 Views
  • 1 replies
  • 0 kudos

Problem with custom Application Template

By following this guide (https://touchgfx.zendesk.com/hc/en-us/articles/115002741432-Create-custom-Application-Template) I have made an custom application template for our hardware. I'm able to select my application template in TouchGFX Designer (4....

MLind by Associate II
  • 2137 Views
  • 4 replies
  • 1 kudos

Change Painter with Animation

Hello community,i want to know if there is a easy way to change the Painter for a Shape (Circle) with an Fade Animation.I can programmatically change the Color. Now i want to Fade the Color Change. The alternative idea is to put a second Circle on to...

LSobo.1 by Associate II
  • 1238 Views
  • 1 replies
  • 0 kudos

TouchGFX lib Binary contains debug info?

Hello, I was looking at the microcontroller binary of a project that I'm using the touchgfx library and something is getting my attention. There is a big part of the file that contains a lot of code information from the touchgfx library. I don't thin...

0693W000001slKKQAY.png
SGold by Associate II
  • 2354 Views
  • 4 replies
  • 0 kudos

STM32Discovery kit for STM32F750 Value Line MCU

Hi,Iam using STM32F750 8-DK Evaluation kit, STM32CudeIDE1.2.0, and STM32Cube_FW_V1.15.0 is SDK. If iam trying to load the LTDC example available in Examples/LTDC/LTDC_Display_1Layer, iam not finding anything on the screen. It is just a blank screen. ...

SMadh.1 by Associate
  • 660 Views
  • 0 replies
  • 0 kudos