STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! DMA2D throws configuration error

Hello!We are use STM32H747 and TouchGFX. We are need to use DMA2D. But we have issue with mode DMA2D_R2M.Our configuration hdma2d.Instance = DMA2D; hdma2d.Init.Mode = DMA2D_R2M; hdma2d.Init.ColorMode = DMA2D_OUTPUT_ARGB8888; hdma2d.Init.Output...

VLesc.1 by Associate
  • 1631 Views
  • 3 replies
  • 0 kudos

Resolved! The problem of touchgfx transplantation of stm32l4r9

(1) The GUI displays an exception. The problem can not be determined. It is suspected that the data sent by dma2d is incorrect. At present, there is no touchgfx fill interface function???(2) Close the GUI display function, directly call the bottom dm...

0693W00000ANrUyQAL.png 0693W00000ANrTCQA1.jpg 0693W00000ANrW1QAL.png
Zlian.1 by Associate II
  • 2401 Views
  • 6 replies
  • 0 kudos

Problem with QSPI and TOuchGFX

Hello!I have homemade board with STM32F746, memory - n25q128.Project generated by Cube 5.5 and touchGFXDesigner 4.13 IDE - KEil 5.29I put one button to main screen.When I put images to internal flash - all works very well.But when I put it to QSPI - ...

0690X00000DAC2fQAH.png
EEuge by Senior
  • 1971 Views
  • 4 replies
  • 0 kudos

TOUCHGFX4.16.1 run target failed

...  Compile       make -f ../gcc/Makefile -j8       Reading TouchGFX/application.config       Linking TouchGFX/build/bin/target.elf       Producing additional output formats...         target.hex  - Combined internal+external hex         intflash.el...

dchen.2 by Associate
  • 1545 Views
  • 2 replies
  • 0 kudos

Hello, I am developing an application of about 20 screens I am trying to find a solution to this problem: how to call a general error screen without having to do it in the code of each screen

I am trying to find a solution to this problem: how to call a general error screen (application hardware failure) from my RTOS code without having to do it in the code of each screen ?Thanks for any clue or solution

SCAYL.1 by Associate
  • 1084 Views
  • 1 replies
  • 0 kudos