User Activity

The latest version of STM32CubeMx 6.6.1 organizes the parameters of the FDCAN differently from the previous version and shows useful information on Time Quantum, Time for one Bit and Baud Rate.But I think the displayed parameters are wrong, as shown ...
Form TouchGFX Designer 4.18.1 I created a simple application.I imported the project into the STM32CubeIDE (1.9) and added support for FreeRTOS.I have selected TIM7 as the timebase source.After calling TouchGFXGeneratedHAL::initialize() in file TouchG...
I try to add external loader to C:\ST\STM32CubeIDE_1.8.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.100.202110141430\tools\bin\ExternalLoaderIn debug configuration, check ExternalLodaer and than press Scan.Th...
My HW:NUCLEO-F446RECustom DISPLAY Board (TFT ILI9314, TPC TSC2007, SPI FLASH MX25R6435F)My SW:X-CUBE-TOUCHGFX 4.17.0STM32CubeIDE Version: 1.6.1STM32Cube_FW_F4_V1.26.1FreeRTOS 10.3.1 with CMSIS_V2Randomly and after some time (from 20 minutes to severa...
I would need to implement what is described in the attached image.Somehow I should "save" which button was pressed so that if the Pin/Password is correct go to the right screen.How can I do ?
Kudos from