STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Slide screen transition problem

I created two screens and did the actions to change the screen. But changing the screen does not work correctly.Added an extra buffer for animationuint16_t buf_ram [160*128];using namespace touchgfx;namespace {  LOCATION_PRAGMA("TouchGFX_Framebuffer"...

VKost.3 by Associate II
  • 8853 Views
  • 11 replies
  • 0 kudos

Changes require to display graphic on the vertical drawing pixel( vertical bytes orientation e.g. display driver SSD1309 etc.).

Hi, I have successfully implemented a complete graphic to display some system related parameter on a monochrome OLED Display with display driver SSD1322, which is a horizontal drawing pixel, however porting the same code to a monochrome OLED Display...

JChou.1 by Associate III
  • 1496 Views
  • 0 replies
  • 0 kudos

Resolved! Without networking, 4.18.0 does not respond

After opening 4.18.0. It stops working after being idle for a period of time, or after creating a new project, or after clicking on some blank areas, and there is no response. How to solve this? (the networked computer is normal, and the non networke...

Zwei.9 by Associate III
  • 2545 Views
  • 5 replies
  • 0 kudos

DSI Video mode refresh error

My project is based on touchgfx using DSI video mode with double buffer. When set the background, part triangle area cannot be refresh. The DSI video configured as the example project of "LCD_DSI_VideoMode_DoubleBuffering".

ZYu.3 by Associate
  • 2838 Views
  • 4 replies
  • 0 kudos