User Activity

I am aware of this discussion:https://community.st.com/s/question/0D53W00000uYapRSAS/how-can-we-iterate-containers-inside-a-container-ie-nested-containerIn my setup I made a custom container called messageBanner.In its constructor, it creates and add...
Most of the sample shows how to add these ranges to the Wildcard Range0-9,A-Z,a-zHow does one add punctuation chars into the Typography using TouchGFX designer?. period ? question mark ! exclamation point .. etcAdding it as comma separators in Wildca...
My platform is STM32H735G-DK and I am trying to test access tothe MX25LM51245G Octo SPI flash. I am using the BSP_OSPI_NOR API that comes with the STM32CubeH7_SDK (version 1.8.0)Test steps:1. At boot, initialize the controller and configure it for me...
Version: Touch GFX Designer 4.16.1Project is attached.My question is similar to:https://community.st.com/s/question/0D50X0000AFpwBx/can-you-call-a-method-on-view-from-a-custom-containerI looked at the ContainerCallback example that Martin posted and ...
version: touchGFX Designer 4.16.1I generated a ScrollList to contain 8 itemsIn the .touchGFX project (attached) I can see the expected lines"Type": "ScrollList", "PaddingBefore": 0, "PaddingAfter": 0, "Snapping": false, "IsHorizontal": false, "IsCirc...
Kudos from