STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

How to return to the last screen view?

If I have multiple parent views with a single child view, is there any good way to return to the caller parent view from a child view?My current implementation is to store the current parent view in the model.cpp class before transitioning to child v...

Rroma.1 by Associate II
  • 1493 Views
  • 2 replies
  • 0 kudos

Questions regarding DataGraphs

I have two questions regarding TouchGFX graphs:1) I have a scroll graph: touchgfx::GraphWrapAndOverwrite<100> graph;The API documentation for GraphWrapAndOverwrite includes a section titled "Protected Functions inherited from AbstractDataGraph", w...

DSwea.1 by Associate III
  • 763 Views
  • 1 replies
  • 0 kudos

Resolved! Run Target error

I solved the previous problem with the TouchGFX compile error.Now I have another problem when I run target.Please see the below link that I made it.https://youtu.be/dDcpmdoovik--------------------------------------------------------------------------...

Resolved! How to flash a board using a bash/python script

Hi,I'm using an STM32L496G board, currently flashing it through CubeMX/Touchgfx Designer.In the future, i'd like to be able to flashthe board by running a bash/python/other script from a linux machine. The board will be connected to the linux machine...

CHech.1 by Associate III
  • 5266 Views
  • 4 replies
  • 0 kudos