Does anyone know why you can't integrate a Touch-GFX project with STM32 Cube on the STM32F7508-DK board.
When I create the project on Touch-GFX and then import the project to the the STM32 Cube IDE , it build fine but when I run the program on the STM32F7508-D board it just becomes a white blank screen. When I click on the reset button it goes back to what it was last programmed to. It looks like it is not writing to the flash or something. Its an issue that is only board specific by the looks of it, since I have tried doing the same on the STM32F769I-DISCO and it works fine ?