User Activity

Hi everyone!In my project, I use TIM2, TIM3, TIM4, TIM5, in each Timer module I choose PWM Input on CH1, and PWM Generation on CH3 function. My goal is to generate PWM pulse at channel 3 and feed back to PWM Input on CH1 to measure Duty cycle and fre...
Hi everyoneMaybe this is an old question but I'm still having troubleI am working on a project on STM2F429 discovery board, now I have to use a larger sized screen for my project.So how do I do it with the correct sequence?What parameters do I need t...
Hello everyone!I'm working on a TouchGFX project on an STM32F429i discovery boardWhen creating project automatically, the default clock source selected in my project is HSE clock source with HCLK frequency of 168Mhz, the program works fine. But when ...
Hello everyone!I'm working on a TouchGFX project on STM32F429 discovery board, because of the small size of the internal flash I have used SD card module with SPI communication standard to store the images.Steps I follow these videos https://www.yout...
Hello everyone!I want to create a TouchGFX project using IAR Workbench. When creating the code with the STM32CubeMX software, I chose EWARM. But when I open the project with IAR workbench, in the workspace there is no gui and generated folder (I want...
Kudos from