User Activity

Hi, We are trying to to read and write to a SD card. We are using the STM32F50N8. Find below attached the schematic for the SD card and the GPIO. We have set it up the same we as mentioned here (SD 4 bit wide mode) - https://www.youtube.com/watch?v=I...
I have tried turning these pins to GPIO's and tried toggling them, however, they seem to just be floating. I can confirm that these pins have been soldered on properly, since I have checked them using an X-RAY inspection system. I can also confirm th...
When I create the project on Touch-GFX and then import the project to the the STM32 Cube IDE , it build fine but when I run the program on the STM32F7508-D board it just becomes a white blank screen. When I click on the reset button it goes back to w...
Selected Device only in the USB_OTG_HS menu. (Made sure that all the pin were set as expected from the schematic).In Middle ware I set Virtual Port Com in the USB_DEVICE section. The project builds fine, but my computer does not recognise any new po...
Kudos from
Kudos given to