STM32 MCUs TouchGFX and GUI

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

TouchGFX Academy launch announcement!

Dear Community, We're excited to announce the creation of the TouchGFX Academy! The TouchGFX Academy is a new place to learn TouchGFX with concrete examples and to find answers to your questions when developing your UI. It includes tutorials of cour...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

determine which button was pressed on a screen

I have two buttons on Screen1.  Both interactions change screen to Screen2.  Can I determine which button was pressed when in Screen2View::setup?Or do I need to use a separate virtual functions and then create a variable setting the button called? 

FJB2069 by Associate II
  • 244 Views
  • 7 replies
  • 0 kudos

IAR Project generation issues

Hello,I'm experiencing issues with TouchGFX file/folder generation.Below the steps I've followed and issues encountered:Create and generate CubeMX project (NUCLEO-U545RE-Q) with TouchGFX, ThreadX and SPI for IAROpen touchgfx.part file, add some text ...

George.P by Associate III
  • 288 Views
  • 4 replies
  • 0 kudos

TouchGFX does not build.

When I install TouchGFX and run the Designer to run the example code, the build fails with an error as shown below.=======================================================================================Compile    make -f ../gcc/Makefile -j10     Read...

STM32H750 discovery not working

Hello, I just bought a STM32H750B-DK and when i tried to flash a sample application from TouchGFX, i got a white screen and the usb programming is not working anymore. I connected via External PowerSupply and STLINK and i can see the board and flash ...

BHure.1 by Associate III
  • 762 Views
  • 5 replies
  • 0 kudos

TouchGFX limitations

Hi,We have a system as below and we have proved that the whole design works fine with TouchGFX framework.However, we are now evaluating if touchGFX is really sufficient for our full requirements. are there any known limitation with touchGFX ? from th...

srig_0-1732548000751.png
srig by Associate
  • 249 Views
  • 3 replies
  • 1 kudos