STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Questions about text management : how can I separate the texts and the fonts in the touchgfx text resources?

Hi,Imagine I want to write the same string in two screens with a font X, with a font Y in another screen, and with a font Z in three other screens, how should I go about it with the current text management that offers touchgfx? Should I just create v...

0693W00000QMAdBQAX.png
GMeur by Senior II
  • 1215 Views
  • 1 replies
  • 0 kudos

Explore more about various features of UI library.

I have gone through the online documentation and user manual but some of the information are not available publicly.You are requested to guide us to fill the below details:CPU Performance:Hardware Acceleration Performance:3D Screen Support:Longevity ...

DTriv.1 by Associate
  • 1381 Views
  • 2 replies
  • 0 kudos

UnmappedDataFont compile error

Hello,I'm using the version 16.1 of TouchGFX and when I generate the project on the simulator I get these error messages when I try to run the code in VS :I generate the project with the following text config: Any help is more than welcome.

0693W00000QMlcFQAT.png 0693W00000QMlcKQAT.png
GMeur by Senior II
  • 861 Views
  • 1 replies
  • 0 kudos

Resolved! How do ILI9806E DSI move?

I am working on a test on the stm32f469i_Discovery board.On the stm32f469i, the MIPI interface operates with the OT8009A LCD. Instead of OT8009A LCDs, it is planning to connect the stm32f469 with other LCDs.The LCD control IC uses the ILI9806E while ...

PKunK.1 by Associate III
  • 8697 Views
  • 7 replies
  • 0 kudos