STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! TouchGFX NEMA Libraries

Hello,We are in the process of integrating TouchGFX into our workflow and back-end build systems. We are using a STM32U599. Please see my question with respect to the tree belowWhat is the difference between TouchGFXNema and NemaGFX libraries?What do...

desmond by Associate III
  • 4770 Views
  • 4 replies
  • 0 kudos

Resolved! Images and fonts dump from elf file

Hi all,we have successully used an external SPI memory to store images.We have defined an external Flash section in our linker file ExtFlashSection :{*(ExtFlashSection ExtFlashSection.*)*(.gnu.linkonce.r.*). = ALIGN(0x4);} >SPI_FLASH and then extract...

SafeDev by Associate II
  • 2850 Views
  • 4 replies
  • 0 kudos

TouchGFX integration with External Project

Hi there, I'm coming across some issues with respect to Touch GFX and my project. I'm trying to build a UI on the Touch GFX Designer software such that it can display certain temperature readings onto the Riverdi STM32H7 embedded display. I'm trying ...

Screenshot 2024-02-23 134717.png Screenshot 2024-02-23 135448.png Screenshot 2024-02-23 135601.png Screenshot 2024-02-23 142905.png

Resolved! TGFX 4.23.2 broke tc declaration in old project

I tried to integrate a working project for version 4.23.0 to 4.23.2 and get the current error as seen in screenshot.I tried to troubleshoot by generating a default project via TGFX to my stm32h7b3I -EVAL board (with a 480x480 screen and GT911 touch d...

Can you use Touch GFX with make?

Hi, I've been trying for a while to put together a simple program that uses both a GUI and an ADC. Previous programs I've made have been built using a text editor and make, but now trying to get toughGFX working in a project, it seems like I need an ...

MLync.4 by Associate II
  • 7622 Views
  • 9 replies
  • 0 kudos