User Activity

I am trying to read multiple ADC channels using the Stm32l072 microcontroller, but in CubeMX, the options for rank assignments, which I normally use to read the channels, are not available. After manually adding these rank assignments to the init fun...
I have stm32f769i discovery card. I want to install a 7 inch 800px 480px screen on this card instead of a 4 inch 800e 480 screen. What adjustments need to be made for this?I can change the resolution via cubemx but I don't know how to do it for inch.
Hello, I'm using a dynamic graph for a project. Can I display 2 different sets of data on this graph? Using 2 separate graphs doesn't solve my problem since I need them to be on the same graph.
Hello guys, I have a question. I am using touchgfx. When I use the while loop in my Model.Cpp file, the application stops. It does this without entering the while loop. Can't use loops in Model.Cpp? Do you have any knowledge about this topic?
hello, i have a problem. When I make my LWIP configurations and try to ping my development board over the computer, I see a different address, not the IP address I set for my card. What is the reason of this? Do you have an idea?When I ping the IP ad...
Kudos given to