cancel
Showing results for 
Search instead for 
Did you mean: 

Flex Button Example with STM32F746G or STM32F7508DK

IGomesMSc
Associate II

Hi everyone,
A simple question, I'm using TouchGFX 4.22 with the example "Flex Button Example" for F746G and F7508.

When the program is set to F746 is not possible look all functions of the UART module... See "DinaF746.png"

But if the program is set to F7508 I look and acess all functions of the UART module... See "DinaF7508.png"

What I do need set in TouchGFX or CubeIDE to solve this problem?

Thank you for help.

IGomes

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
MM..1
Chief III

This is nothing to do with Touch or STM type. Showing this "inteli" is based on setup in IDE for indexing and build...

for example How to turn on auto fill ( auto complete ) in STM3... - STMicroelectronics Community

View solution in original post

4 REPLIES 4
MM..1
Chief III

You have reply on your png HA_ isnt HAL_

and why you mark this as touchgfx???

Hi I attach the correct figure now
my application I'll use F746G TouchGFX and UART integration...

And we really like the TouchGFX

MM..1
Chief III

This is nothing to do with Touch or STM type. Showing this "inteli" is based on setup in IDE for indexing and build...

for example How to turn on auto fill ( auto complete ) in STM3... - STMicroelectronics Community

Perfect, thanks for the quick response and attention...