STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! setup round display

(Moved from Feedback to the TouchGFX forum) Hi there TouchGFX team! How can I setup a round display and develop the UI for it? I haven't decided yet on the display but I just want to make TouchGFX can work with round displays Thanks a lot in advance

JPabl.1 by Senior
  • 1746 Views
  • 3 replies
  • 1 kudos

Resolved! STM32F423ZHT6- ST7789H2

I sent a write data to LCD like display the RED background on the LCD panel. But it display like this-    this is my code part: int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration---------------------------------...

LCD image.jpeg
Meenakshi by Associate III
  • 2683 Views
  • 8 replies
  • 0 kudos

Resolved! QR Code Feature issue in TouchGFX 4.24

Hello , i am working for the first time on TouchGfx and learning step by step some basics about it . I currently encountred a problem with QR Code Feature . If i put an URL Link longer than 17 characters ,it wont be shown after i run the simulation ....

akdou by Associate
  • 1596 Views
  • 3 replies
  • 2 kudos

Resolved! How to use the circle progress?

Hi,I want to show a circle progress like below:In touchgfx's circleProgress, there is't the little circle at the progress line end;So I am drawing the little circle and update its position realtime;Is there any simpler way to do the same things?And m...

Junde_1-1729159898639.png
Junde by Senior III
  • 1939 Views
  • 3 replies
  • 1 kudos