User Activity

Hello! I have a question that was raised before, but didn't get an answer:  https://community.st.com/t5/stm32-mcus-touchgfx-and-gui/what-if-number-of-data-points-is-greater-than-number-of-pixels/m-p/222692Basically, my question is the same but concer...
Hello!I need to be able to enable and disable touch screen from my GUI application. I don't want to cut the power to the touchscreen.I want my handle click functions on multiple screens to not to respond to touch events for some time after certain po...
Hello! I have a problem with simulator. When switching between screens (no animation) simulator crashes. The finalizeTransition function returns, after that the application ticks one time, and then crashes. Everything is executed normally on the targ...
Hello! Please, help me to recover from designer crush.I open my .touchgfx file in the designer (4.22.0), and it opens fine, but with a yellow dot next to Texts tab. (I re-installed some fonts that were used by the application before). But when I pres...
Hello! I have a following problem: I use Designer to generate some screens, and some screens I create without designer. When I create a custom screen (not the screen that I draw in designer) I create two folders:include/gui/my_screen (with myView.hpp...