User Activity

Hi all,I currently working on a project using TouchGFX, multiple tasks are using functions from <math.h> which are not re-entrant, so I have them mutex protected. The drivers using these functions are written in C.Does anyone know if the TouchGFX lib...
Hello,I recently purchased the STM32U5G9J-DK2, on the pre-loaded demo there is a map view which takes advantage of the vector graphics acceleration.The demo is "TouchGFX Demo 7", but the version available in Designer v4.23.0 is missing the map screen...
Hello,In the annex video it is mentioned that the project archive is available for the Nucleo board project with X-NUCLEO-IKA01A1, however when I download the materials archive it appears to be missing.Could you confirm this is the case, if so would ...
Hello,Are there plans to fully support the STEVAL-PROTEUS1 board in NanoEdge AI Studio? Currently only the STEVAL-STWINKT1B has full support (with datalogging).Many thanks,Anthony
Hi,I'm interested in working with ML and AI on STM32, after spending some time looking through ST documentation I think using NanoEdge AI Studio + ST board is the quickest way to help me understand things.From what I can see, the latest available fun...