STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1797 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4942 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9688 Views
  • 5 replies
  • 3 kudos

Resolved! Speed monitoring and Single stepping a motor

I am running a 28 pole 20A nominal motor using x-Nucleo IHM08M1 and a nucleo -G431RB. I have been doing a number of tests verifying locked rotor current/torque and checking the effect of different settings of proportional gain. I am using Stm32CubeMo...

Resolved! STEVAL-CTMV009V1 3ICS.

Hi, st team,mcsdk: 6.2.1control board: nucleo-g474reBridge: XNUCLEO-IHM09M2Power Board: STEVAL-CTM009V1We're going to buy around 10k-25k uc per year.1. STEVAL-CTM008V1 schematic diagram defines that it is possible to use 3 ICS. 2. X-NUCLEO-IHM09M2 ci...

tezz_1-1710157997673.png tezz_2-1710158039410.png tezz_0-1710157831120.png
tezz by Associate
  • 1614 Views
  • 2 replies
  • 0 kudos

Resolved! NUCLEO-H503RB motor drive USART communication

Hi, ST community.I'm trying to drive a motor using Nucleo-H503RB. At that time, I am trying to change the USART pin of STLINK and connect it to Motor pilot, but it does not connect.<Detail>I want to use PB14 and PB15 for the STLINK USART pins instead...

Kota by Associate
  • 2567 Views
  • 3 replies
  • 2 kudos

B-G431GB-ESC1 can't run Motor Profiler

Hi everyone, I want to simply use the B-G431GB-ESC1 evaluation board for making a model of my 3-phase brushless DC motor:https://dk.rs-online.com/web/p/dc-motorer-jaevnstromsmotorer/2163791?gb=sAs for now I just want to flash the evaluation board wit...

danielschultzen_0-1709150621213.png danielschultzen_1-1709151288859.png

Resolved! X-Nucleo-IHM07M1 Voltage

I have the X-Nucleo-IHM07M1 siting on top of NUCLEO-F302R8 as shown attached. Trying to connect as follow? It is possible to connect 24V onto this board to drive 24V 3 phase motor?  

Theng_0-1710002899709.png
Theng by Associate II
  • 1460 Views
  • 1 replies
  • 1 kudos

UART 4 bit numeric value communication

I am doing the project to control linear motor, For that I am using UART to send start and stop command to start and stop motor, as like this i sending different rpm value from 100 to 3000 randomly to change the ramp of the motor. The problem that i ...

soundarya_h_s_0-1709892543564.png

motor control

I need to purchase a motor development kit, does ST provide it? Including control board, drive, etc. Thank you

LEUNG by Associate II
  • 1425 Views
  • 1 replies
  • 0 kudos

Resolved! cannot select dual motors in MotorControl Workbench 6.1.2

I am having issues selecting 2 motors when creating a new project using 6.1.2.  the dropdown box only displays "1".  this functionality seems to work in workbench 5.4.8.  All of the documentation say to just select the number of motors.  I am new to ...

DougD by Associate
  • 1832 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.