STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1735 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4882 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9582 Views
  • 5 replies
  • 3 kudos

Motor profiler does not connect NUCLEO-F746ZG and X-NUCLEO-IHM08M1 3Sh Workbench connects but cannot spin the motor

I am using the NUCLEO-F746ZG and X-NUCLEO-IHM08M1 3Sh configuration and try to run the motor Profiler. However, the programming seems to run properly, the connection to the board does not seems to work. I got the warning : The FW embeeded on control ...

SBACO by Associate III
  • 1208 Views
  • 4 replies
  • 0 kudos

Resolved! My question is : can the C produced by the ST Motor Control Workbench be modified by to permit all 3 inverter currents to be measured by the same ADC, for example ADC 1? This would result in a 200ns delay for the 2nd measurement, and 400ns delay for 3rd

Messieurs,I am using the ST NUCLEO-F303RE together with an X-NUCLEO-IHM08M1 and the ST Motor Control Workbench (STMCW) to drive a BLDC motor using ST code.In addition, my company has designed its own motor control board for driving two BLDC motors us...

PBroo.2 by Associate
  • 1851 Views
  • 3 replies
  • 0 kudos

Resolved! Can I use Position control with Hall Sensor with SPIN-3201?

Hi, I am new to the Motion Control system.and I have SPIN-3201 with a BLDC motor.It is hard to apply ST Motor Control Workbench 5.4.6.because the version of STM32CubeIDE and some Setting of the Project(error of FOC duration and Start-up failure)anywa...

LYS by Associate II
  • 2671 Views
  • 4 replies
  • 0 kudos