cancel
Showing results for 
Search instead for 
Did you mean: 

No FreeRTOS for 6-step with kit P-NUCLEO-IHM03?

bitschubser
Associate

Hi there,

I am new to motor control and I am trying to set up my P-Nucleo-IHM03 kit with MC Workbench 6.1.2. I would like to use FreeRTOS in combination with the 6-step algorithm but in the "Application Configuration" under "FreeRTOS" it is stated: "Selected hardware boards do not support this feature".

I was wondering why FreeRTOS is not supported in this case?

With the *same hardware* and the FOC algorithm selected there is no such statement and I am having no issues generating a FreeRTOS project. So for 6-step I would now try to add FreeRTOS in STM32CubeMX, but I would like to know if there is any adamant obstacle that would prevent the combination of 6-step with FreeRTOS either in hardware or the 6-step library?   

Thanks  

   

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Zied b.
ST Employee

hello @bitschubser , Sorry to answer so late, indeed the FreeRtos is not supported by the 6-steps because the algorithm has not been adapted for the activation of the FreeRtos unlike the FOC, it is however possible to activate it on CubeMx but you risk losing the functioning of the motor control, because the synchronization of the tasks will not be done correctly.
You can try to adapt the 6-step algorithm but it's still hard work.

Regards

If you agree with my answer, please accept it by clicking on "Accept as solution".

View solution in original post

1 REPLY 1
Zied b.
ST Employee

hello @bitschubser , Sorry to answer so late, indeed the FreeRtos is not supported by the 6-steps because the algorithm has not been adapted for the activation of the FreeRtos unlike the FOC, it is however possible to activate it on CubeMx but you risk losing the functioning of the motor control, because the synchronization of the tasks will not be done correctly.
You can try to adapt the 6-step algorithm but it's still hard work.

Regards

If you agree with my answer, please accept it by clicking on "Accept as solution".