STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1742 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4891 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9591 Views
  • 5 replies
  • 3 kudos

STSPIN32F0 Incompatible Pinout

I have made a custom 24V drive using the STSPIN32F0 chip. For the first take on this board, I have followed the STEVAL-SPIN3201 design. I have changed the gain values for the op-amps, the MOSFETS, and a few signal inputs to the MCU. I have the custom...

rjack by Associate II
  • 1567 Views
  • 0 replies
  • 0 kudos

Resolved! Board Manager "busVoltageDivider" issues

I'm having issues with the "busVoltageDivider" property in the "VBusSensing" feature.The Wiki says that the "VBusSensing" feature doesn't define any global propery, however the Board Manager is complaining that the property is missing when I don't ad...

DMeie.2 by Senior II
  • 1569 Views
  • 1 replies
  • 0 kudos

Profiler Control Parameters

I am trying to drive a 250W BLDC motor. I started profiling the motor, which looked promesing. I based a project on the motor characteristics, but haven't been able to drive the motor as well as the motor profiler did. I have used same drive frequenc...

2800rpm.png 2800rpm_noise.png 2800rpm_OC.png

How to upload STEVAL-ESC002V1?

I bought a STEVAL-ESC002V1 board and I don't know how to customize its firmware. I downloaded STM32CUDE IDE and Motor Control Workbench but none of than have a board option for STEVAL-ESC002V1 nor STSPIN32F0A. So, I downloaded the STSW-ESC002V1 which...

ACho.11 by Associate II
  • 1706 Views
  • 1 replies
  • 0 kudos

Regarding motor low RPM not achieved

I have a BLDC motor equipped with Hall sensors. When attempting to run the motor in FOC (Field-Oriented Control) mode, I encountered difficulties achieving the required low RPM. Consequently, I configured the Hall sensors to run the motor, but encoun...

suhas1 by Associate II
  • 1441 Views
  • 1 replies
  • 0 kudos

Evspin32G4-dual : Turning 2 motors simultaneously

Hello,I have an EVSPIN32G4-Dual, I am Trying to Run 2 HooverBoard Motors (36V/15A/510RPM/HALL).I generated the firmware using Mc Workbench 6.2.1 and desabled the overcurrent protection for stage 2. Then tried to command the motors using motor pilot, ...

ItzSam by Associate II
  • 1738 Views
  • 2 replies
  • 0 kudos

Motor is not spinning

Dear all,I have a NUCLEO-F302R8 and the X-NUCLEO-IHM07M1 motor driver expansion board. I have a three phase BLDC motor with an encoder attached to it. I have profiled the motor and I am able to run the motor in the profiler. When I use the workbench ...

nonameX by Associate
  • 1455 Views
  • 1 replies
  • 0 kudos