Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello. I have been messing around with the STMF407VG for a few weeks now using a discovery board. Been the steep learning curve but I think I have made significant progress on learning firmware development on it. I have gotten my code to be to a poin...
I tried to modify firmware of ST-Link of NUCLEO-L053R8 using a tutorial.However, when I select CMSIS-dap in Keil (as mentioned in tutorial) it says "not a genuine ST device abort connection". Everything worked well before modification.Now I want to r...
Hi, We are using a customized board with stm32l4x MCU. A QSPI flash is connected with MCU. Trying to program qspi flash using ST Link Utility with External Loader. Somehow we are able to manage to program the qspi flash. Problem statement is, if I do...
Hey, I try to connect to STM32G0316-Discovery board from STM32 ST-Link Utility but no connection can be etablished. Err-Message is: "Can not connect to target! Can't reset the core."Software is okay, driver is okay (other boards work), onboard stlink...
Hello, I bought a NUCLEO-L552ZE-Q and tried to connect with STLINK Utility . But STLINK Utility rejects.08:57:29 : ST-LINK SN : 066CFF505352716587121640 08:57:29 : V2J37M26 08:57:29 : Connected via SWD. 08:57:29 : SWD Frequency = 4,0 MHz. 08:57:29 ...
We're using the STM32 Nucleo-L4R5ZIThe issue is that whenever we try to check the ST-Link using STM32Cube Programmer or ST-Link Utility, it won't connect to the board.We kept getting errors like"STLink USB Communication Error""No STM32 Target Found"I...
Attached please is the connected equipment, installed software and the error message.
Should be a fairly easy one, but wanted to ask first: the built in T_VCP_RX and T_VCP_TX show the opposite logic input/output to what I'd expect (Rx shows as an output) in table 6 of the user manual UM2502. So would I connect my target Rx pin to the...