2019-10-20 10:38 AM
Was able to program the board previously, but today after updating my STM32CubeIDE, it refused to run debug until I updated the stlink on my dev board.
But upon doing so, it gave these error. Essentially meaning I cannot program my dev board.
```
STMicroelectronics ST-LINK GDB server. Version 5.3.2
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.2.0
-------------------------------------------------------------------
Log output file: /tmp/STM32CubeProgrammer_TqQf5t.log
ST-LINK SN : 002F001F3137511233333639
ST-LINK FW : V3J4M2
Voltage : 3.28V
SWD freq : 24000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Cannot identify the device
Error: unknown or unsupported device (DevID = 0x0000)
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_QKNgwM.srec
File : ST-LINK_GDB_server_QKNgwM.srec
Size : 157296 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.199
Verifying ...
Error: Data mismatch found at address 0x08000004 (byte = 0x31 instead of 0x5D)
Error: Download verification failed
Encountered Error when opening /Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.macos64_1.1.0.201910081157/tools/bin/STM32_Programmer_CLI
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
```
I am running this IDE on a mac on MacOS catalina. Oh and btw I still cannot run latest STM32CubeProgrammer on mac, even after updating java to latest version.
2019-10-20 10:49 AM
Would probably edge back the speed from 24 MHz, and select most verbose logging.
Try setting the BOOT0 switch to 1-System Mode
2019-10-20 9:19 PM
No problems here.
STMicroelectronics ST-LINK GDB server. Version 5.3.2
Copyright (c) 2019, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.2.0
-------------------------------------------------------------------
Log output file: C:\Users\hansd\AppData\Local\Temp\STM32CubeProgrammer_a09124.log
ST-LINK SN : 002000463137510939383538
ST-LINK FW : V3J4M2
Voltage : 3.29V
SWD freq : 24000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Device name : STM32H7xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a09124.srec
File : ST-LINK_GDB_server_a09124.srec
Size : 69496 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:01.258
Verifying ...
Download verified successfully
The funny thing is Cube Programmer offers version V3J3M2 and ST Link Utility V3J4M2???
Anyway try Cube Programmer with a reduced speed.
2019-10-20 9:20 PM
Sorry, I should mention I have the poor man's version Nucleo-H743I2.
2019-10-20 9:55 PM
There is now a new option with ST Link Server to set SWD speed. Not sure how to use it with CubeIDE yet. There should really be a selection box like in CubeProgrammer.
--frequency <max freq kHz>
Specifies the ST-LINK communication frequency in kHz, such as 5, 25, 100, 240, 950, 1800, 4000, 8000,
24000 kHz.
2019-10-20 11:31 PM
Yeah there is a way to change the swd speed. Just tried 5Khz to no success... so not too sure what changed between the old version and this version of STLink
/Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.macos64_1.1.0.201910081157/tools/bin/STM32_Programmer_CLI -c port=swd freq=5 reset=HWrst mode=UR
-------------------------------------------------------------------
STM32CubeProgrammer v2.2.0
-------------------------------------------------------------------
ST-LINK SN : 002F001F3137511233333639
ST-LINK FW : V3J4M2
Voltage : 3.28V
SWD freq : 5 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Cannot identify the device
Error: unknown or unsupported device (DevID = 0x0000)It would be nice if STM32CubeIDE allowed me to use an older version of STLink.
2019-10-21 1:27 AM
Okay just rediscovered the windows only stlink GUI utility STSW-LINK004 from:
Turns out that the windows STSW-LINK004 utility works and was able to erase the board. However I was still not able to access the board from my mac using STM32CubeIDE. I wonder if it's to do with any change in stlink debug configuration between the old STM32CubeIDE and the new STM32CubeIDE.
Btw how did you get "STM32CubeProgrammer" working? I've already tried it on Mac, Linux, Windows with no luck. Is it requiring a specific java version?
Ok, going to try making a new STM32CubeIDE project to see if it's anything to do with the project migration.
2019-10-21 1:48 AM
Just created a new CubeMX project named `testproj` and kept it to all the default values and just ran it in STM32CubeMX on my mac. Still failed.
Looks like something is wrong with the inbuilt`STM32CubeProgrammer v2.2.0` in STM32CubeIDE for `stm32H743-EVALv2`. But the windows STSW-LINK004 stlink GUI utility works... so maybe windows STM32CubeIDE would work?
2019-10-22 12:27 PM
I think I'm running into this as well - see here
2019-10-22 1:10 PM
I have the same issue. With F303 Discovery and STM3240G-EVAL. Running mac os sierra and STM32CubeIDE Version: 1.1.0. Everything worked fine before updating