STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STLINK-V3MINI Serial Pinout Question

Should be a fairly easy one, but wanted to ask first: the built in T_VCP_RX and T_VCP_TX show the opposite logic input/output to what I'd expect (Rx shows as an output) in table 6 of the user manual UM2502. So would I connect my target Rx pin to the...

STM32H747XI Power Scheme

Hello everyone,I am desining a new board with STM32H747XI and i am stuck with power schematic.As i see, this mcu has internal smps regulator and we can use it several way but not as vdd supplier.I am cunfused about it. Can anyone help me thougt this?...

I am using a STM32G071. If I connect a STLINK to the uC, and then I disconnect it, also after a reset cycle, BOOT0 pin status is ignored and the boot happens always on Flash Memory instead of System Memory. Why? Is it normal?

I want to use BOOT0 pin to select System Memory boot.nBOOT0 = 0, nBOOT1 = 1, nBOOT_SEL = 0 bits in user config are well programmed. Boot works well if my uC is coming from a POR or power cycle. But if I connect a ST-LINK to the uC and simply open the...

ATPG by Associate II
  • 2110 Views
  • 2 replies
  • 0 kudos

Resolved! ST-LINK_CLI.exe issue : Programming Failed

The Command is " ST-LINK_CLI.exe -c id=0 swd lpm crst -P "JM.bin" -V after_programming -score "When I do Program SM32f765 Using Device St-Link V2 & STM32Cube programmer GUI , then every time it is programmed .while randomly i get the issue with STli...

PJain.1 by Associate
  • 3759 Views
  • 3 replies
  • 0 kudos