STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stlink v3 Absolutely awful?

This tool only supports 5 breakpoints!Orginal and cloned versions of j-link have a lot more ability!I can not believe!Only 5 breakpoints are not useful at all in the debugging environment!Because of my interest in st company, while I have four other ...

kshin.111 by Associate III
  • 1639 Views
  • 4 replies
  • 0 kudos

How to check the date code on IC

Hi STMicroelectronic,I have the MCU pard number STM32F101RCT6 and I would like to know the date code of this IC.The markking on the IC show 815 but I am not sure it mean from 2008 or 2018. see picture as attached.Could you please advise on this?

0693W000008wNqNQAU.jpg
RAnan.1 by Associate
  • 4802 Views
  • 5 replies
  • 1 kudos

Resolved! Problem with ADC Vrefint monitoring.

Hello. A have my custom board with STM32G431CBU microcontroller. Power domain on my board are shown in the picture:I want to measure the voltage on Vref+ pin. The analog domain settings of CubeMX are:The code for single ADC acquisition:HAL_ADC_Start(...

0693W000008wB9HQAU.png 0693W000008wBAeQAM.png 0693W000008wB9DQAU.png
EAlek.11 by Associate II
  • 7133 Views
  • 6 replies
  • 0 kudos

Resolved! After unplugging ST-Link and reconnecting it I get: Error in initializing ST-LINK device. Reason: (4) No device found on target.

I'm using the STM32H735G DK eval board. Was able to load my code and use the FDCAN ok, when I went on to get the SD-Card going, I found that when reading a block the first 12 bytes would not be transferred. Since I have two boards and so tried the se...

HSamm.1 by Associate II
  • 1820 Views
  • 2 replies
  • 0 kudos