MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DH impact detection

Posted on March 01, 2014 at 10:23HelloI have read that impact detection functionality can be performed by LIS3DH. I am unable to find any information on HOW to configure the device for impact detection.Is it identical to ''click'' detection? If no -...

igor2 by Associate II
  • 669 Views
  • 0 replies
  • 0 kudos

LSM9DS0 +16g range

Posted on February 26, 2014 at 11:06I've set up the LSM9DS0 to the +/-16g range by setting AFS2 - 0 as 100 as per datasheet. Normal g comes out as 0.7g, yet all other ranges are fine. What am I doing wrong? Chris

clock stability, and sampling rate on LSM9DS0

Posted on October 26, 2013 at 09:15There are no figures for clock stability over time and temperature. These are going to effect the sample rate times. For example, if the accelerometer DOR is 100Hz, what spread can be expected. I take it that in al...

Configuring LIS3DH

Posted on February 20, 2014 at 08:31I connected LIS3DH in the following way , but the device does'nt give the correct reading.          What is wrong with this configuration? Vin = 3.3V, SPI 4 wires. I configured the registers with the following str...

yohai by Associate
  • 1664 Views
  • 3 replies
  • 0 kudos

LSM330 vs LSM330DLC

Posted on January 27, 2014 at 07:06Hello, what is the difference between these two modules? Why DLC is so much expensive? #lsm330 #lsm330 #lsm330dlc

L3G4200D gyro

Posted on February 23, 2014 at 06:04The description page of the L3G4200D gyroscope says that it is an angular rate sensor able to provide unprecedented stablility of zero rate level and sensitivity over temperature and time. Does that mean that ther...

Question about LIS3DH FIFO

Posted on February 12, 2014 at 17:44HelloI am trying to use the LIS3DH in FIFO Mode with Filter enabled.In this mode, the X-Axis, and Y-Axis values get some normal values (they oscillate between -10 and +10) but the Z-Axis value seems to have a bypa...

avieira by Associate II
  • 2168 Views
  • 5 replies
  • 0 kudos

LIS3DH datasheet error?

Posted on December 16, 2013 at 14:53In LIS3DH datasheet (Doc ID 17530) on table 25 we can see: Default value 00     ODR3-0 (0000:50Hz Others:...) on table 26 we can see: 0000 Power down mode So what is ODR = 0000  Power down or 50Hz? #lis3dh

Mich1 by Associate III
  • 888 Views
  • 1 replies
  • 0 kudos