User Activity

Posted on December 30, 2013 at 11:32Hello! I have a STM32L151CB and I need to use the UART interface. At first it worked perfectly, but after I changed the system clock from HSI (16 MHz) to MSI (2 MHz) I only receive some characters. E.g. when I sen...
Posted on October 08, 2014 at 14:09Hello How many bit does the data output of the LSM330 have? I can't find it in the datasheet. The register is 2x8 bit long, but are all bits valid? Regards Daniel #lsm330
Posted on September 24, 2014 at 13:18Hello How many packets can the BlueNRG send in a single connection event? I need this information to estimate the possible throughput. Thanks!