MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DH wrong behavior after writing to CTRLREG6

Posted on November 18, 2014 at 19:53Hello,Some day ago I've started work with LIS3DH accelerometer. Everything works fine -Reading accelerations, highpass filter, low power mode and INT1 interrupt line.At start INT1 was configured as high when activ...

radoslaw by Associate
  • 632 Views
  • 0 replies
  • 0 kudos

impat detection using lis3dsh sensor.

Posted on November 15, 2014 at 08:55hi i m using lis3dsh sensor to detect the accidents. for this i need to detect the impact using the variation of the G value.. from sudden shift of 2g to around 16 g and also fall detection .. so far i am getting ...

n.serina by Associate III
  • 663 Views
  • 0 replies
  • 0 kudos

Data ready interrupt on lsm303d

Posted on November 14, 2014 at 20:55Hi i was trying to enable the data ready on accelerometer .however i'm not sure how to check whether it's enabled or not .i mean whenever i read the value in IG_SRC2 it shows that 0x00 also i have not enabled the ...

iNEMO-M1 as SPI Slave

Posted on November 03, 2014 at 15:44Hello EveryoneI am working with the STEVAL-MKI121V1 board and Discovery-M1-Fw package, trying to get rid of the USB interface and replace it with SPI configured as Slave. My intention  for the the final system is ...

rasko by Associate
  • 879 Views
  • 1 replies
  • 0 kudos

PCB design guidelines

Posted on November 03, 2014 at 23:45Hello, I'm developing a compass module based on the LSM303D with a STM32F030x as host controller. I'm a little bit confused about the inconsistent PCB guidelines and application hints. In the application hints se...

marten by Associate II
  • 993 Views
  • 0 replies
  • 0 kudos

LSM330D Self Test

Posted on October 21, 2014 at 16:28According to it's datasheet the LSM330D has a self test mode enabled by setting the self-test bit to 1 however there is no register entry I can find dor the self-test bit.Where is it ?

rhunt by Associate
  • 914 Views
  • 1 replies
  • 0 kudos

LSM330DL - DataRready Interrupt

Posted on November 20, 2013 at 10:38Hi community, i am working on an application with the accelerometer and gyroscope in LSM330DL. At the moment I try to use the DataReady-Interrupt for the gyroscope. My understanding of DRDY-Interrupt is that when...

pz by Associate II
  • 2716 Views
  • 6 replies
  • 0 kudos

LSM303D anti-alias filter

Posted on October 31, 2014 at 21:54I'm a bit lost about the use of the acceleration filter bandwidth. How to choose the relevant value between 50 and 773Hz ? -- Fabien #filter #lsm303d #accelerometer