using self test feature of LIS3DSH
Posted on January 19, 2015 at 10:35how can i manage the self test in LIS3DSH.after enabling this option what i do? where can i found the result of test?
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Posted on January 19, 2015 at 10:35how can i manage the self test in LIS3DSH.after enabling this option what i do? where can i found the result of test?
Posted on June 13, 2014 at 10:07after power up the LIS2DM the current consumption is about 100uA ?!The connection is:Pin1 : SCL with a external 4K7 to 3VPin2 : SDA with a external 4K7 to 3VPin3 : SA0 connected to GNDPin4 : /CS connected to 3VPin5: I...
Posted on February 15, 2014 at 11:59Hi, I am looking for SPI driver interface for magnetometer LSM303D thanks #lsm303d-spi-driver
Posted on March 17, 2015 at 13:38Does ST have any mems engineers?.... specifically an expert on the LSM303??? I'm having hardware issues with this part...(it is connected properly, board layout 100%, spi interface working.....not a hobby/hack deal.....
Posted on March 16, 2015 at 16:21The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on March 12, 2015 at 23:32The original post was too long to process during our migration. Please click on the attachment to read the original post.
Posted on December 23, 2014 at 16:39I have installed UNICO v4.0 to acquire data from the STEVAL-MKI154V1 accelerometer/gyro. However, it seems I am unable to establish a connection with the evaluation kit. The STMicro Virtual COM Port appears in the...
Posted on March 10, 2015 at 10:18It took me a while to understand it, but the datasheet for the LIS3DSH chip is dead wrong. It's a pretty obvious copy/paste mistake while creating that datasheet from another chip, but there is no such thing on that ...
Posted on March 09, 2015 at 19:36I was able to get the 6d movement detection working and below I have the register configurations that I've done.My application logic is to configure for normal fifo mode and after a certain application delay switch t...
Posted on March 06, 2015 at 10:29Hello,Does anybody knows what is the start up time of LSM9DS0 chip? I am having a problem that chip is sending the same data from accelerometer or gyroscope all the time and I have to reset the device and it is work...