MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

INEMO-M1 I2C1 address

Posted on April 14, 2015 at 15:04Hi in the documentation you wrote that the INEMO-M1 can be addressed as slave by the I2C1 port. How can we do this? I can't found the slave address for the INEMO module in the documentation Is the INEMO firmware alr...

pascal2 by Associate
  • 968 Views
  • 0 replies
  • 0 kudos

iNemo custom board

Posted on April 12, 2015 at 21:12Hi, I have developed, printed and mounted a custom iNemo based board: I noticed a short circuit between Vcc and Gnd with my multimeter, so my question is: there is an hidden problem in my circuit (like a short circui...

daniel23 by Associate II
  • 670 Views
  • 0 replies
  • 0 kudos

STEVAL-MKI121V1 with STM32F4

Posted on April 02, 2015 at 23:15Hello guys, I'm a newbie so forgive me if my question is stupid.I'm trying to get the values that the gyroscope of  i-nemoreturns  and i want to send them through SPI to a STM32F4 ... how can I do?

sinatra by Associate
  • 627 Views
  • 0 replies
  • 0 kudos

LIS3DH Interrupts - can't clear threshold interrupt

Posted on April 01, 2015 at 15:19I've got a LIS3DH interrupting on a threshold. I went by the example in CD00290365.pdf for a filtered example, operating on a >300mg threshold.My problem is when it interrupts. The int line is held low for one output...

tau by Associate II
  • 780 Views
  • 0 replies
  • 0 kudos

Self test output change for LIS331DLH

Posted on October 16, 2013 at 18:02Hi, We have developed a product which uses the LIS331DLH accelerometer and are happy with the results so far. My issue concerns the self test output change which can be higher than stated in specifications. The dat...

mgrelet by Associate
  • 1493 Views
  • 3 replies
  • 0 kudos

VL6180X supply voltage

Posted on March 26, 2015 at 15:40The VL6180X's typical supply voltage is listed as 2.8V.  Is there any problem with operating it at 3.3V which is less than the 3.6V absolute maximum?

tlock by Associate
  • 899 Views
  • 1 replies
  • 0 kudos

LSM330DLC and LSM303DLHC sensitivity and offset

Posted on March 24, 2015 at 15:13Hello, In both the datasheets of the LSM330DLC and LSM303DLHC, it is indicated that a factory calibration is performed and its results are stored in the device (both sensitivity and offset). Where are these registers...

jean23 by Associate
  • 776 Views
  • 0 replies
  • 0 kudos

LSM303DTR pitch roll lock up on startup

Posted on March 05, 2015 at 18:58we are using the LSM303DTR.  4 wire spi. we initialize CONFIG 1,CONFIG5 and CONFIG 7 only....assuming defaults on all others. on power up, we get the pitch and roll always returning 0x8008 (our gui displays this as -...

jyoung2 by Associate
  • 904 Views
  • 1 replies
  • 0 kudos

LSM303D Z-axis Direction

Posted on March 23, 2015 at 23:28Why if the LSM303D a steady-state on a horizontal surface measures 0 g on the X-axis and 0 g on the Y-axis, whereas the Z-axis measures 1g = 1000mg?Direction of  Z detectable accelerations is upward (see pag. 8/52 Do...